This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TDA2P-ABZ: timestamp in SBL

Part Number: TDA2P-ABZ
Other Parts Discussed in Thread: TDA2

Tool/software: TI-RTOS

Hi All,

I am using VSDK 3.05. We have a requirement where we need to toogle a GPIO within 100ms of power up, i.e we need to toggle it in SBL. I have included csl_gpio.h in sbl_tda2xx_main.c. I have pin muxed the gpio inside the function SBLConfigTIEVMPad()

After this I have toggled the gpio. Now I need to see whether that gpio is toggled within 100ms. Is there any api or any method to see this apart from using scope.

Regards,

Deepika

  • Hi Deepika,

    You can read 32K Timer for the same.
    The counter starts from 0 at power up and the same is used by SBL for profiling.

    Regards,
    Rishabh
  • Hi Rishabh,

    Can you please refer to any example present in Vision SDK. Is it the timer register mentioned in sec 24.3 in the TRM ( 32-kHz Synchronized Timer (COUNTER_32K)). If that is not the case please let me know the exact register to read.

    Regards,
    Deepika

  • Hi Deepika,

    Yes I am referring to COUNTER_32K.

    Regards,
    Rishabh
  • Hi Deepika,

    Also you can directly call SBLUtilsRead32KTimer API as used by SBL.

    Regards,
    Rishabh
  • Hi Rishabh,

    The return type of this function is integer. What is its unit?

    Regards,
    Deepika
  • Deepika,

    The return type is unsigned integer.
    See SblPrintBootCycles API for conversion to milliseconds.

    Regards,
    Rishabh
  • Hi Deepika,

    Were you able to get the timestamp?

    Regards,
    Rishabh
  • Hi Rishabh,

    Thanks for the reply.
    I have added the following lines after the function SBLConfigTIEVMPad() :

    GPIOModuleEnable(SOC_GPIO1_BASE);
    GPIODirModeSet(SOC_GPIO1_BASE,TDA_LED0_GPIO1_26,GPIO_DIR_OUTPUT);
    GPIOPinWrite(SOC_GPIO1_BASE, TDA_LED0_GPIO1_26, GPIO_PIN_HIGH);
    timeValGpioToggleEnd=SBLUtilsRead32KTimer();
    SblPrintBootCycles("Time at which gpio Toggled ", timeValGpioToggleEnd);

    I am getting the following output

    Time at which gpio Toggled - 19363 (1.65 ms)

    Now is this time after system start up ?
    How to identify this?

    Thanks
    Deepika
  • Deepika,

    What is the type for timeValGpioToggleEnd? It should be uint32_t.
    The calculation should give you 590.91 ms.
    I am not sure why you are not getting this.
    SBL profiling is done using the same API.

    Regards,
    Rishabh

  • Hi Rishabh,

    The type is uint32_t only.
    I have checked another function ARM_CCNT_Read().Can I try this?

    Also based on your inputs right now if it takes 590ms , is it possible to toggle a gpio within 100ms.



    Regards,
    Deepika

  • Hi Deepika,

    I missed that you are using TDA2Px and not TDA3xx, my bad.
    I will get back to you on this.

    Regards,
    Rishabh
  • Hi Deepika,

    You can use TIMER_32K on TDA2Px as well.
    Yes you can toggle GPIO well within 100 ms.
    It depends on lot of factors like boot mode, SBL execution, UART prints etc.
    You need to make sure that you run the code in such a way that you can meet 100 ms requirement.
    Similar time stamp mechanism is already implemented in TDA2P SBL for getting IPU1_0 start time.

    Regards,
    Rishabh
  • Hi Rishabh,

    I am using SBLUtilsRead32KTimer () and SblPrintBootCycles() as shown above and the time is showing 1.67 ms. Is this the time after start up?

    Right now I am using SD booting.

    Regards,
    Deepika
  • Deepika,

    Can you share the complete SBL log.

    Regards,
    Rishabh
  • Hi Rishabh,

    Please find the logs below,this is for a custom TDA2P board.

    TDA2Px SBL Boot

    DPLL Configuration Completed

    Clock Domain Configuration Completed

    Module Enable Configuration Completed

    TI EVM PAD Config Completed

    TDA2Px DDR Configuration

    DDR Config Completed

    *****************************************************************

    SD Boot - file open completed successfully

    MPU CPU0 Image Load Completed

    IPU1 CPU0 Image Load Completed

    IPU1 CPU1 Image Load Completed

    DSP1 Image Load Completed

    DSP2 Image Load Completed

    EVE1 Image Load Completed

    EVE2 Image Load Completed

    App Image Download Completed

    Putting MPU CPU1 in Off mode

    EVE MMU configuration completed

    EVE MMU configuration completed

    *****************************************************************

    PMCCNTR counts once every 64 clock cycles, multiple by 64 to get actual CPU cycles

    SBL Initial Config Cycles - 1742534  (148.69 ms)                            

    SOC Init Cycles - 205823  (17.56 ms)

    DDR Config Clock Cycles - 95837  (8.17 ms)

    App Image Load Cycles - 117493703  (10026.12 ms)

    Slave Core Bootup Cycles - 137065  (11.69 ms)

    SBL Boot-up Cycles - 119682810  (10212.93 ms)

    Time at which SBL started IPU1_0 - 343418  (29.30 ms)

    Time at which gpio Toggled  - 14173  (1.20 ms)

    *****************************************************************

    Jumping to MPU CPU0 App

    All cores UP[IPU1-0]     10.480448 s:  ***** IPU1_0 Firmware build time 11:47:56 Jan  7 2019

    [IPU1-0]     10.480692 s:  *** SYSTEM: CPU Frequency <ORG = 212800000 Hz>, <NEW = 212800000 Hz>

    [IPU1-0]     10.568687 s:  SYSTEM: Notify register to [IPU1-1] line 0, event 15...

    [IPU1-0]     10.568901 s:  SYSTEM: Notify register to [DSP1] line 0, event 15...

    [IPU1-0]     10.568992 s:  SYSTEM: Notify register to [DSP2] line 0, event 15...

    [IPU1-0]     10.569114 s:  SYSTEM: Notify register to [EVE1] line 0, event 15...

    [IPU1-0]     10.569236 s:  SYSTEM: Notify register to [EVE2] line 0, event 15...

    [IPU1-0]     10.569328 s:  SYSTEM: Notify register to [HOST] line 0, event 15...

    [IPU1-0]     10.571097 s:  *** UTILS: CPU MHz = 20 Mhz ***

    [IPU1-0]     10.571280 s:  SYSTEM: System Common Init in progress !!!

    [IPU1-0]     10.582931 s:  SYSTEM: IPC init in progress !!!

    [IPU1-0]     10.583053 s:  SYSTEM: Notify init done !!!

    [IPU1-0]     10.585127 s:  SYSTEM: MsgQ init done !!!

    [IPU1-0]     10.585310 s:  SYSTEM: IPC init DONE !!!

    [IPU1-0]     10.590678 s:  SYSTEM: System Common Init Done !!!

    [IPU1-0]     10.590831 s:  SYSTEM: System Init in progress !!!

    [IPU1-0]     10.590922 s:  SYSTEM: BSP Common Init in progress !!!

    [IPU1-0]     10.591014 s:  SYSTEM: BSP Common Init Done !!!

    [IPU1-0]     10.591075 s:  SYSTEM: BSP Platform Init in progress !!!

    [IPU1-0]     10.591258 s:  SYSTEM: BSP Platform Init Done !!!

    [IPU1-0]     10.591349 s:  SYSTEM: FVID2 Init in progress !!!

    [IPU1-0]     10.591502 s:  SYSTEM: FVID2 Init Done !!!

    [IPU1-0]     10.591593 s:  SYSTEM: VPS Init in progress !!!

    [IPU1-0]     10.591654 s:  SYSTEM: VPDMA Descriptor Memory Address translation ENABLED [0xa0000000 -> 0x80000000]

    [IPU1-0]     10.595223 s: *** VPDMA Firmware Loading... ***

    [IPU1-0]     10.595345 s: VPDMA Firmware Address = 0x9fd1b5c0

    [IPU1-0]     10.595437 s: VPDMA Load Address     = 0x4897d004

    [IPU1-0]     10.595589 s: VPDMA Firmware Version = 0x4d0001b8

    [IPU1-0]     10.595681 s: VPDMA List Busy Status = 0x00000000

    Can you please tell me why does SBL Initial Config Cycles takes 148ms

    Regards,

    Deepika

  • Deepika,

    Let's first try to resolve the timestamp issue.
    I see one problem here that needs to fixed in TDA2 SBL for IPU timestamp value.
    SblPrintBootCycles API has different implementation for TDA2xx and TDA3xx.
    When you are reading 32K timer you need to use implementation given in TDA3 SBL.
    As an experiment can you replace the implementation of this API with the one given in TDA3 SBL.
    You will correct timestamp although other time profiling will be wrong.

    Regards,
    Rishabh
  • Hi Rishabh,

    "When you are reading 32K timer you need to use implementation given in TDA3 SBL.As an experiment can you replace the implementation of this API with the one given in TDA3 SBL."

    I did'nt understood this

    So should I remove all the ARM_CCNT_Read() and use SBLUtilsRead32KTimer () in sbl_tda2xx_main.c

    Correct me if I am wrong

    Regards
    Deepika
  • Deepika,

    SblPrintBootCycles is defined in sbl_tda3xx_main.c and sbl_tda2xx_main.c.
    You need to replace the API definition given in sbl_tda2xx_main.c with the one given in sbl_tda3xx_main.c

    Regards,
    Rishabh
  • Hi Rishabh,

    With this I am getting a linker error. I cleaned it again.

    I added stdio.h and in snprintf function I modified the format specifier with %ld instead of %d
    snprintf(bootCyclesStr, (size_t) 8, "%ld", bootCycles);

    /home/deepika/FFC_sensor/scripts/..//sdk/ti/PROCESSOR_SDK_VISION_03_03_00_00/ti_components/cg_tools/linux/gcc-arm-none-eabi-4_9-2015q3/arm-none-eabi/lib/fpu/librdimon.a(rdimon-syscalls.o): In function `_sbrk':
    syscalls.c:(.text._sbrk+0x78): undefined reference to `end'
    collect2: error: ld returned 1 exit status


    Regards,
    Deepika
  • Hi Deepika,

    Use the below definition:

    uint32_t cyclesInMsInt = 0U, cyclesInMsFrac = 0U;
    
    cyclesInMsInt = (bootCycles * 1000U) / SBL_32KTIMER_REFERENCE_VAL;
    
    cyclesInMsFrac =
        (((bootCycles * 1000U) % SBL_32KTIMER_REFERENCE_VAL) * 100U) / SBL_32KTIMER_REFERENCE_VAL;
    
    UARTprintf("\n %s - %d  (%d.%02d ms)",
               cyclesString, bootCycles, cyclesInMsInt, cyclesInMsFrac);

    Regards,

    Rishabh

  • Hi Rishabh,

    Now it worked according to your expectations:

    SBL Initial Config Cycles - 1761638 (53760.92 ms)
    SOC Init Cycles - 205475 (6270.59 ms)
    DDR Config Clock Cycles - 95777 (2922.88 ms)
    DDR test Wait time Clock Cycles - 0 (0.0 ms)
    App Image Load Cycles - 124934131 (11599.10 ms)
    Slave Core Bootup Cycles - 136908 (4178.10 ms)
    SBL Boot-up Cycles - 127141766 (78970.77 ms)
    Time at which SBL started IPU1_0 - 368912 (11258.30 ms)
    Time at which gpio Toggled - 18850 (575.25 ms)

    Now tell me how you can I reduce this Gpio toggling time.


    Regards,
    Deepika

  • Deepika,

    Glad that this issue is resolved.
    Can you add a new API for getting time stamp for ipu1_0 and gpio with the provided definition so that you can see SBL profiling numbers correctly along with correct time stamps.
    Reducing boot time is not a straight forward action and cannot be done by some register configuration.
    Also please start a new thread for boot time reduction.

    Regards,
    Rishabh
  • HI Rishabh,

    Time at which SBL started IPU1_0------timeValStartIpu1_0 is already available in the present file.Can you please let me know what else can I add for ipu1_0.

    Regards,
    Deepika
  • Deepika,

    There are two places where 32K Timer will be used. One for ipu1_0 that was already there and the other you have added for gpio.
    At both places you need to use the API definition I provided you in this thread say SblPrintBootCycles32K.

    Regards,
    Rishabh
  • Hi Rishabh,

    Thanks a lot for your support. I have reverted to the original TI SDK code, with that the time has been reduced further to 332 ms.
    I will open a thread to reduce the boot time further.

    This is what I am currently getting :

    SBL Initial Config Cycles - 116409 (9.93 ms)
    SOC Init Cycles - 170606 (14.55 ms)
    DDR Config Clock Cycles - 89616 (7.64 ms)
    App Image Load Cycles - 96433659 (8229.0 ms)
    Slave Core Bootup Cycles - 130417 (11.12 ms)
    SBL Boot-up Cycles - 96941763 (8272.36 ms)
    Time at which SBL started IPU1_0 - 281181 (8580.96 ms)
    Time at which gpio Toggled - 10884 (332.15 ms)
    *****************************************************************

    Regards,
    Deepika
  • Deepika,

    Thanks for the confirmation.
    I am closing this thread.

    Regards,
    Rishabh