Hello,
I'd like to connect DM365's AEMIF to DM6446's HPI and preserve NAND functionality on DM365. My idea is to use current CE0 to select the NAND chip and connect CE1 to DM6446's HPI along with required signals. But since the NAND chip on EVM board is 3.3v , DM6446's HPI power supply is 1.8v. I am not sure if change to 1.8v NAND chip (such as change to K9F5608U0C), Can DM365 boot normally?