Part Number: TMS320C6678
Hi,
After filling up the power calculation excel sheet, I got following current consumption number for CVDD power rail:
Total = 16A
Baseline = 10A
Activity = 6A
From the datasheets and app notes, I know that the baseline current portion is not all DC; it has AC components too. I need to know what is the transient current (AC) from these numbers to calculate AC target impedance for PDN decoupling analysis. How can we get the transient current portion from the above numbers?
Regards,
Binayak