This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TCIEVMK2X: Is it possible to read GPIO with 1us resolution ?

Other Parts Discussed in Thread: 66AK2L06

Tool/software: Linux

Hi

I am using 66AK2L06 Evaluation modüle with arago linux distribution.

We try to determine pulse width -nearly 1us in length-

İs it possible ?

  • We try to read gpio with "gpio_read()" function (see below)

    We call this function in the infine loop.

    Is it possible to detect 1us pulse  ?



    int gpio_read(gpio_t *gpio, char *value) { char buf[2]; /* Read fd */ if (read(gpio->fd, buf, 2) < 0) return _gpio_error(gpio, GPIO_ERROR_IO, errno, "Reading GPIO 'value'"); /* Rewind */ if (lseek(gpio->fd, 0, SEEK_SET) < 0) return _gpio_error(gpio, GPIO_ERROR_IO, errno, "Rewinding GPIO 'value'"); if (buf[0] == '0') *value = 0; else if (buf[0] == '1') *value = 1; else return _gpio_error(gpio, GPIO_ERROR_IO, 0, "Unknown GPIO value"); return 0; }