I am trying to help a customer select a new NAND Flash for the DM355. His present Flash, the MT29F16G08DAAWP, is going obsolete and Micron recommended the MT29F16G08ABABAWP as a replacement. The problem is that the recommended part doesn't appear to be supported by the DM355 RBL (the DM355 won't boot). This brings up a few questions:
1) SPRUFB3 (page 160) lists the compatible NAND Flash by (single byte) Device ID, but I can't seem to find the Device ID in the Flash datasheet (maybe I'm just missing it?). As I understand SPRUFB3 this byte is read from the Flash and compared to the table. If the datasheet doesn't list the device ID then I can't say for sure if the device is supported or not.
2) Is there a list available that correlates the Device ID in SPRUFB3 to manufactures P/N?
3) The forum indicated that the RBL would be updated from time-to-time. Does anyone know when the next update will be? Does anyone know what the new device ID table will look like, i.e. what Flash devices will be supported?
4) Lacking item 2, can anyone recommend a Flash to replace the one going obsolete (MT29F16G08DAAWP) that is also in the table?
Thanks!