Part Number: PROCESSOR-SDK-AM335X
Tool/software: Linux
Hello I'am trying to build arago-base-tisdk-image using this steps (checked from scratch multiple times):
# Host - Ubuntu 16.04 - 64 bit
sudo apt-get install git build-essential python diffstat texinfo gawk chrpath dos2unix wget unzip socat doxygen libc6:i386 libncurses5:i386 libstdc++6:i386 libz1:i386
sudo dpkg-reconfigure dash
# say NO
wget https://releases.linaro.org/components/toolchain/binaries/7.2-2017.11/arm-linux-gnueabihf/gcc-linaro-7.2.1-2017.11-x86_64_arm-linux-gnueabihf.tar.xz
tar -Jxvf gcc-linaro-7.2.1-2017.11-x86_64_arm-linux-gnueabihf.tar.xz -C $HOME
wget https://releases.linaro.org/components/toolchain/binaries/7.2-2017.11/aarch64-linux-gnu/gcc-linaro-7.2.1-2017.11-x86_64_aarch64-linux-gnu.tar.xz
tar -Jxvf gcc-linaro-7.2.1-2017.11-x86_64_aarch64-linux-gnu.tar.xz -C $HOME
git clone git://arago-project.org/git/projects/oe-layersetup.git tisdk
cd tisdk
./oe-layertool-setup.sh -f configs/processor-sdk/processor-sdk-05.02.00.10-config.txt
cd build
. conf/setenv
export TOOLCHAIN_PATH_ARMV7=$HOME/gcc-linaro-7.2.1-2017.11-x86_64_arm-linux-gnueabihf
export TOOLCHAIN_PATH_ARMV8=$HOME/gcc-linaro-7.2.1-2017.11-x86_64_aarch64-linux-gnu
MACHINE=am335x-evm bitbake arago-base-tisdk-image
Build fails with message:
ERROR: libtool-cross-2.4.6-r0 do_configure: configure failed
ERROR: libtool-cross-2.4.6-r0 do_configure: Function failed: do_configure (log file is located at /home/andrey/data/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/libtool-cross/2.4.6-r0/temp/log.do_configure.6007)
File log.do_configure.6007:
...
checking for arm-linux-gnueabi-gcc... arm-linux-gnueabihf-gcc -march=armv7-a -marm -mfpu=neon -mfloat-abi=hard --sysroot=/home/andrey/data/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/libtool-cross/2.4.6-r0/recipe-sysroot
checking whether the C compiler works... no
configure: error: in `/home/andrey/data/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/libtool-cross/2.4.6-r0/build':
configure: error: C compiler cannot create executables
See `config.log' for more details
...
File config.log:
...
configure:3815: checking whether the C compiler works
configure:3837: arm-linux-gnueabihf-gcc -march=armv7-a -marm -mfpu=neon -mfloat-abi=hard --sysroot=/home/andrey/data/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/libtool-cross/2.4.6-r0/recipe-sysroot -isystem/home/andrey/data/gcc-linaro-7.2.1-2017.11-x86_64_arm-linux-gnueabihf/arm-linux-gnueabihf/include -O2 -pipe -g -feliminate-unused-debug-types -fdebug-prefix-map=/home/andrey/data/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/libtool-cross/2.4.6-r0=/usr/src/debug/libtool-cross/2.4.6-r0 -fdebug-prefix-map=/home/andrey/data/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/libtool-cross/2.4.6-r0/recipe-sysroot-native= -fdebug-prefix-map=/home/andrey/data/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/libtool-cross/2.4.6-r0/recipe-sysroot= -isystem/home/andrey/data/gcc-linaro-7.2.1-2017.11-x86_64_arm-linux-gnueabihf/arm-linux-gnueabihf/include -L/home/andrey/data/gcc-linaro-7.2.1-2017.11-x86_64_arm-linux-gnueabihf/arm-linux-gnueabihf/lib -Wl,-rpath-link,/home/andrey/data/gcc-linaro-7.2.1-2017.11-x86_64_arm-linux-gnueabihf/arm-linux-gnueabihf/lib -Wl,-O1 -Wl,--hash-style=gnu conftest.c >&5
/media/andrey/data/gcc-linaro-7.2.1-2017.11-x86_64_arm-linux-gnueabihf/bin/../lib/gcc/arm-linux-gnueabihf/7.2.1/../../../../arm-linux-gnueabihf/bin/ld: cannot find ../../lib/libc.so.6
...
So, configutaion fails because cross-compiler can't find libc.so.6.
Indeed, libc.so.6 is broken symbolik line to libc-2.25.so (Look at screenshot)
In my previous builds on virtual machine this directory containde files lib<XXX>-2.25.so copied from cross-compiler dir:
gcc-linaro-7.2.1-2017.11-x86_64_arm-linux-gnueabihf/arm-linux-gnueabihf/libc (Look at screenshot)
Why the cross compiler libs are missing? Thanks!