This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM335X: AM335X DDR Timing waveform/model

Part Number: PROCESSOR-SDK-AM335X

We have designed PCB of SOM using AM335X for Ethernet communication.

We are doing signal integrity analysis on the board.But for  SI analysis of the DDR bus ,we donot found any timing information in the datasheet.

We are using  HyperLynx,it uses the DDR Wizard for which one of the requirement is the timing model of the DDR Controller.

Parameters required:

1. tCKAC (pre-launch delay, CK to Address and Command signals),

2 tCKCTL(pre-launch delay, CK to Control signals), 

3 tCKDQS(Output delay or skew, CK output to DQS output), 

4 tDQSDQ(pre-launch delay, DQS output to DQ and DM outputs)

and tDQDQS(Tolerable input skew between DQS and DQ).

So pl. provide the timing parameter listed above for analysis.

 

  • Hemant, we do not provide timing information to support timing simulations for DDR. Instead, we have detailed DDR layout guidelines (provided in the datasheet), which if followed, will provide enough timing margin for a successful design. Timing parameters will comply with JEDEC standards.

    Regards,
    James