This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM3505: CVE-2017-5715 and CVE-2017-5753

Part Number: AM3505

Tool/software: Linux

Hi,

I am using AM3505 Processor and I am using 4.9 kernel.

Did Armv7 affected with  bounds check bypass, Spectre-V1, Spectre 1.0 and branch target injection, Spectre-V2.

 if yes then is there any fix is available for these two CVE.CVE-2017-5753 (bounds check bypass, Spectre-V1, Spectre 1.0) and CVE-2017-5715 (branch target injection, Spectre-V2)

As per my researc In opensource kernel i checkout the linux-4.9-y branch and i search above two CVE. then i got below commits for these two cve.

CVE-2017-5715

there are two commits for this particular CVE Fix.

c9ae3d5717bf14c05299f184c4bfee79e9a22efe

a3d6dd6a66c1bf01a36926705db4687c7d0d4734

CVE-2017-5753

there are two commits for this particular CVE Fix.

012df71d2980d9ddf8039da09b2d5741189da8f1

a9bfac14cde2b481eeb0e64fbe15305df66ab32e

Question: Is above commits are sufficient for fixing CVE-2017-5715 and CVE-2017-5753 in am3505 (cortex A8,ARMv7) ??

if not can you please suggest me to how i can proceed or is there any additional patches availabe for am3505 (cortex A8,ARMv7).

CVE-2017-5715

==============

c9ae3d5717bf14c05299f184c4bfee79e9a22efe

commit c9ae3d5717bf14c05299f184c4bfee79e9a22efe
Author: Mark Rutland <mark.rutland@arm.com>
Date:   Thu Apr 12 12:11:31 2018 +0100

    arm64: KVM: Report SMCCC_ARCH_WORKAROUND_1 BP hardening support
    
    
    From: Marc Zyngier <marc.zyngier@arm.com>
    
    commit 6167ec5c9145cdf493722dfd80a5d48bafc4a18a upstream.
    
    A new feature of SMCCC 1.1 is that it offers firmware-based CPU
    workarounds. In particular, SMCCC_ARCH_WORKAROUND_1 provides
    BP hardening for CVE-2017-5715.
    
    If the host has some mitigation for this issue, report that
    we deal with it using SMCCC_ARCH_WORKAROUND_1, as we apply the
    host workaround on every guest exit.
    
    Tested-by: Ard Biesheuvel <ard.biesheuvel@linaro.org>
    Reviewed-by: Christoffer Dall <christoffer.dall@linaro.org>
    Signed-off-by: Marc Zyngier <marc.zyngier@arm.com>
    Signed-off-by: Catalin Marinas <catalin.marinas@arm.com>
    [v4.9: account for files moved to virt/ upstream]
    Signed-off-by: Mark Rutland <mark.rutland@arm.com> [v4.9 backport]
    Tested-by: Greg Hackmann <ghackmann@google.com>
    Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>

diff --git a/arch/arm/include/asm/kvm_host.h b/arch/arm/include/asm/kvm_host.h
index d5423ab..9fe1043 100644
--- a/arch/arm/include/asm/kvm_host.h
+++ b/arch/arm/include/asm/kvm_host.h
@@ -318,4 +318,10 @@ static inline int kvm_arm_vcpu_arch_has_attr(struct kvm_vcpu *vcpu,
        return -ENXIO;
 }
 
+static inline bool kvm_arm_harden_branch_predictor(void)
+{
+       /* No way to detect it yet, pretend it is not there. */
+       return false;
+}
+
 #endif /* __ARM_KVM_HOST_H__ */
diff --git a/arch/arm/kvm/psci.c b/arch/arm/kvm/psci.c
index 1120ad0..3d96225 100644
--- a/arch/arm/kvm/psci.c
+++ b/arch/arm/kvm/psci.c
@@ -403,13 +403,20 @@ int kvm_hvc_call_handler(struct kvm_vcpu *vcpu)
 {
        u32 func_id = smccc_get_function(vcpu);
        u32 val = PSCI_RET_NOT_SUPPORTED;
+       u32 feature;
 
        switch (func_id) {
        case ARM_SMCCC_VERSION_FUNC_ID:
                val = ARM_SMCCC_VERSION_1_1;
                break;
        case ARM_SMCCC_ARCH_FEATURES_FUNC_ID:
-               /* Nothing supported yet */
+               feature = smccc_get_arg1(vcpu);
+               switch(feature) {
+               case ARM_SMCCC_ARCH_WORKAROUND_1:
+                       if (kvm_arm_harden_branch_predictor())
+                               val = 0;
+                       break;
+               }
                break;
        default:
                return kvm_psci_call(vcpu);
diff --git a/arch/arm64/include/asm/kvm_host.h b/arch/arm64/include/asm/kvm_host.h
index e505038..37d56e8 100644
--- a/arch/arm64/include/asm/kvm_host.h
+++ b/arch/arm64/include/asm/kvm_host.h
@@ -393,4 +393,9 @@ static inline void __cpu_init_stage2(void)
                  "PARange is %d bits, unsupported configuration!", parange);
 }
 
+static inline bool kvm_arm_harden_branch_predictor(void)
+{
+       return cpus_have_cap(ARM64_HARDEN_BRANCH_PREDICTOR);
+}
+
 #endif /* __ARM64_KVM_HOST_H__ */
diff --git a/include/linux/arm-smccc.h b/include/linux/arm-smccc.h
index dc68aa5..e1ef944 100644
--- a/include/linux/arm-smccc.h
+++ b/include/linux/arm-smccc.h
@@ -73,6 +73,11 @@
                           ARM_SMCCC_SMC_32,                            \
                           0, 1)
 
+#define ARM_SMCCC_ARCH_WORKAROUND_1                                    \
+       ARM_SMCCC_CALL_VAL(ARM_SMCCC_FAST_CALL,                         \
+                          ARM_SMCCC_SMC_32,                            \
+                          0, 0x8000)
+
 #ifndef __ASSEMBLY__
 
 #include <linux/linkage.h>

a3d6dd6a66c1bf01a36926705db4687c7d0d4734

Author: Alexei Starovoitov <ast@kernel.org>
Date:   Mon Jan 29 02:48:56 2018 +0100

    bpf: introduce BPF_JIT_ALWAYS_ON config
    
    [ upstream commit 290af86629b25ffd1ed6232c4e9107da031705cb ]
    
    The BPF interpreter has been used as part of the spectre 2 attack CVE-2017-5715.
    
    A quote from goolge project zero blog:
    "At this point, it would normally be necessary to locate gadgets in
    the host kernel code that can be used to actually leak data by reading
    from an attacker-controlled location, shifting and masking the result
    appropriately and then using the result of that as offset to an
    attacker-controlled address for a load. But piecing gadgets together
    and figuring out which ones work in a speculation context seems annoying.
    So instead, we decided to use the eBPF interpreter, which is built into
    the host kernel - while there is no legitimate way to invoke it from inside
    a VM, the presence of the code in the host kernel's text section is sufficient
    to make it usable for the attack, just like with ordinary ROP gadgets."
    
    To make attacker job harder introduce BPF_JIT_ALWAYS_ON config
    option that removes interpreter from the kernel in favor of JIT-only mode.
    So far eBPF JIT is supported by:
    x64, arm64, arm32, sparc64, s390, powerpc64, mips64
    
    The start of JITed program is randomized and code page is marked as read-only.
    In addition "constant blinding" can be turned on with net.core.bpf_jit_harden
    
    v2->v3:
    - move __bpf_prog_ret0 under ifdef (Daniel)
    
    v1->v2:
    - fix init order, test_bpf and cBPF (Daniel's feedback)
    - fix offloaded bpf (Jakub's feedback)
    - add 'return 0' dummy in case something can invoke prog->bpf_func
    - retarget bpf tree. For bpf-next the patch would need one extra hunk.
      It will be sent when the trees are merged back to net-next
    
    Considered doing:
      int bpf_jit_enable __read_mostly = BPF_EBPF_JIT_DEFAULT;
    but it seems better to land the patch as-is and in bpf-next remove
    bpf_jit_enable global variable from all JITs, consolidate in one place
    and remove this jit_init() function.
    
    Signed-off-by: Alexei Starovoitov <ast@kernel.org>
    Signed-off-by: Daniel Borkmann <daniel@iogearbox.net>
    Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>

diff --git a/init/Kconfig b/init/Kconfig
index 34407f1..b331fee 100644
--- a/init/Kconfig
+++ b/init/Kconfig
@@ -1609,6 +1609,13 @@ config BPF_SYSCALL
          Enable the bpf() system call that allows to manipulate eBPF
          programs and maps via file descriptors.
 
+config BPF_JIT_ALWAYS_ON
+       bool "Permanently enable BPF JIT and remove BPF interpreter"
+       depends on BPF_SYSCALL && HAVE_EBPF_JIT && BPF_JIT
+       help
+         Enables BPF JIT and removes BPF interpreter to avoid
+         speculative execution of BPF instructions by the interpreter
+
 config SHMEM
        bool "Use full shmem filesystem" if EXPERT
        default y
diff --git a/kernel/bpf/core.c b/kernel/bpf/core.c
index ab9576b..64c4b13 100644
--- a/kernel/bpf/core.c
+++ b/kernel/bpf/core.c
@@ -458,6 +458,7 @@ noinline u64 __bpf_call_base(u64 r1, u64 r2, u64 r3, u64 r4, u64 r5)
 }
 EXPORT_SYMBOL_GPL(__bpf_call_base);
 
+#ifndef CONFIG_BPF_JIT_ALWAYS_ON
 /**
  *     __bpf_prog_run - run eBPF program on a given context
  *     @ctx: is the data we are operating on
@@ -923,6 +924,13 @@ static unsigned int __bpf_prog_run(void *ctx, const struct bpf_insn *insn)
 }
 STACK_FRAME_NON_STANDARD(__bpf_prog_run); /* jump table */
 
+#else
+static unsigned int __bpf_prog_ret0(void *ctx, const struct bpf_insn *insn)
+{
+       return 0;
+}
+#endif
+
 bool bpf_prog_array_compatible(struct bpf_array *array,
                               const struct bpf_prog *fp)
 {
@@ -970,7 +978,11 @@ static int bpf_check_tail_call(const struct bpf_prog *fp)
  */
 struct bpf_prog *bpf_prog_select_runtime(struct bpf_prog *fp, int *err)
 {
+#ifndef CONFIG_BPF_JIT_ALWAYS_ON
        fp->bpf_func = (void *) __bpf_prog_run;
+#else
+       fp->bpf_func = (void *) __bpf_prog_ret0;
+#endif
 
        /* eBPF JITs can rewrite the program in case constant
         * blinding is active. However, in case of error during
@@ -979,6 +991,12 @@ struct bpf_prog *bpf_prog_select_runtime(struct bpf_prog *fp, int *err)
         * be JITed, but falls back to the interpreter.
         */
        fp = bpf_int_jit_compile(fp);
+#ifdef CONFIG_BPF_JIT_ALWAYS_ON
+       if (!fp->jited) {
+               *err = -ENOTSUPP;
+               return fp;
+       }
+#endif
        bpf_prog_lock_ro(fp);
 
        /* The tail call compatibility check can only be done at
diff --git a/lib/test_bpf.c b/lib/test_bpf.c
index 2e38502..98da752 100644
--- a/lib/test_bpf.c
+++ b/lib/test_bpf.c
@@ -5646,9 +5646,8 @@ static struct bpf_prog *generate_filter(int which, int *err)
                                return NULL;
                        }
                }
-               /* We don't expect to fail. */
                if (*err) {
-                       pr_cont("FAIL to attach err=%d len=%d\n",
+                       pr_cont("FAIL to prog_create err=%d len=%d\n",
                                *err, fprog.len);
                        return NULL;
                }
@@ -5671,6 +5670,10 @@ static struct bpf_prog *generate_filter(int which, int *err)
                 * checks.
                 */
                fp = bpf_prog_select_runtime(fp, err);
+               if (*err) {
+                       pr_cont("FAIL to select_runtime err=%d\n", *err);
+                       return NULL;
+               }
                break;
        }
 
@@ -5856,8 +5859,8 @@ static __init int test_bpf(void)
                                pass_cnt++;
                                continue;
                        }
-
-                       return err;
+                       err_cnt++;
+                       continue;
                }
 
                pr_cont("jited:%u ", fp->jited);
diff --git a/net/core/filter.c b/net/core/filter.c
index 4eb4ce0..6e0d17b 100644
--- a/net/core/filter.c
+++ b/net/core/filter.c
@@ -1005,11 +1005,9 @@ static struct bpf_prog *bpf_migrate_filter(struct bpf_prog *fp)
                 */
                goto out_err_free;
 
-       /* We are guaranteed to never error here with cBPF to eBPF
-        * transitions, since there's no issue with type compatibility
-        * checks on program arrays.
-        */
        fp = bpf_prog_select_runtime(fp, &err);
+       if (err)
+               goto out_err_free;
 
        kfree(old_prog);
        return fp;
diff --git a/net/core/sysctl_net_core.c b/net/core/sysctl_net_core.c
index a7f05f0..1b46190 100644
--- a/net/core/sysctl_net_core.c
+++ b/net/core/sysctl_net_core.c
@@ -292,7 +292,13 @@ static struct ctl_table net_core_table[] = {
                .data           = &bpf_jit_enable,
                .maxlen         = sizeof(int),
                .mode           = 0644,
+#ifndef CONFIG_BPF_JIT_ALWAYS_ON
                .proc_handler   = proc_dointvec
+#else
+               .proc_handler   = proc_dointvec_minmax,
+               .extra1         = &one,
+               .extra2         = &one,
+#endif
        },
 # ifdef CONFIG_HAVE_EBPF_JIT
        {
diff --git a/net/socket.c b/net/socket.c
index 05f13b2..bd3b339 100644
--- a/net/socket.c
+++ b/net/socket.c
@@ -2548,6 +2548,15 @@ static int __init sock_init(void)
 
 core_initcall(sock_init);      /* early initcall */
 
+static int __init jit_init(void)
+{
+#ifdef CONFIG_BPF_JIT_ALWAYS_ON
+       bpf_jit_enable = 1;
+#endif
+       return 0;
+}
+pure_initcall(jit_init);
+
 #ifdef CONFIG_PROC_FS
 void socket_seq_show(struct seq_file *seq)
 {

 

CVE-2017-5753

=============

commit 012df71d2980d9ddf8039da09b2d5741189da8f1
Author: Andrew Honig <ahonig@google.com>
Date:   Wed Jan 10 10:12:03 2018 -0800

    KVM: x86: Add memory barrier on vmcs field lookup
    
    commit 75f139aaf896d6fdeec2e468ddfa4b2fe469bf40 upstream.
    
    This adds a memory barrier when performing a lookup into
    the vmcs_field_to_offset_table.  This is related to
    CVE-2017-5753.
    
    Signed-off-by: Andrew Honig <ahonig@google.com>
    Reviewed-by: Jim Mattson <jmattson@google.com>
    Signed-off-by: Paolo Bonzini <pbonzini@redhat.com>
    Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>

diff --git a/arch/x86/kvm/vmx.c b/arch/x86/kvm/vmx.c
index d858290..ab66054 100644
--- a/arch/x86/kvm/vmx.c
+++ b/arch/x86/kvm/vmx.c
@@ -857,8 +857,16 @@ static inline short vmcs_field_to_offset(unsigned long field)
 {
        BUILD_BUG_ON(ARRAY_SIZE(vmcs_field_to_offset_table) > SHRT_MAX);
 
-       if (field >= ARRAY_SIZE(vmcs_field_to_offset_table) ||
-           vmcs_field_to_offset_table[field] == 0)
+       if (field >= ARRAY_SIZE(vmcs_field_to_offset_table))
+               return -ENOENT;
+
+       /*
+        * FIXME: Mitigation for CVE-2017-5753.  To be replaced with a
+        * generic mechanism.
+        */
+       asm("lfence");
+
+       if (vmcs_field_to_offset_table[field] == 0)
                return -ENOENT;
 
        return vmcs_field_to_offset_table[field];
(END)

commit a9bfac14cde2b481eeb0e64fbe15305df66ab32e
Author: Alexei Starovoitov <ast@kernel.org>
Date:   Sun Jan 7 17:33:02 2018 -0800

    bpf: prevent out-of-bounds speculation
    
    commit b2157399cc9898260d6031c5bfe45fe137c1fbe7 upstream.
    
    Under speculation, CPUs may mis-predict branches in bounds checks. Thus,
    memory accesses under a bounds check may be speculated even if the
    bounds check fails, providing a primitive for building a side channel.
    
    To avoid leaking kernel data round up array-based maps and mask the index
    after bounds check, so speculated load with out of bounds index will load
    either valid value from the array or zero from the padded area.
    
    Unconditionally mask index for all array types even when max_entries
    are not rounded to power of 2 for root user.
    When map is created by unpriv user generate a sequence of bpf insns
    that includes AND operation to make sure that JITed code includes
    the same 'index & index_mask' operation.
    
    If prog_array map is created by unpriv user replace
      bpf_tail_call(ctx, map, index);
    with
      if (index >= max_entries) {
        index &= map->index_mask;
        bpf_tail_call(ctx, map, index);
      }
    (along with roundup to power 2) to prevent out-of-bounds speculation.
    There is secondary redundant 'if (index >= max_entries)' in the interpreter
    and in all JITs, but they can be optimized later if necessary.
    
    Other array-like maps (cpumap, devmap, sockmap, perf_event_array, cgroup_array)
    cannot be used by unpriv, so no changes there.
    
    That fixes bpf side of "Variant 1: bounds check bypass (CVE-2017-5753)" on
    all architectures with and without JIT.
    
    v2->v3:
    Daniel noticed that attack potentially can be crafted via syscall commands
    without loading the program, so add masking to those paths as well.
    
    Signed-off-by: Alexei Starovoitov <ast@kernel.org>
    Acked-by: John Fastabend <john.fastabend@gmail.com>
    Signed-off-by: Daniel Borkmann <daniel@iogearbox.net>
    Cc: Jiri Slaby <jslaby@suse.cz>
    [ Backported to 4.9 - gregkh ]
    Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>

diff --git a/include/linux/bpf.h b/include/linux/bpf.h
index 97498be..75ffd3b 100644
--- a/include/linux/bpf.h
+++ b/include/linux/bpf.h
@@ -43,6 +43,7 @@ struct bpf_map {
        u32 max_entries;
        u32 map_flags;
        u32 pages;
+       bool unpriv_array;
        struct user_struct *user;
        const struct bpf_map_ops *ops;
        struct work_struct work;
@@ -189,6 +190,7 @@ struct bpf_prog_aux {
 struct bpf_array {
        struct bpf_map map;
        u32 elem_size;
+       u32 index_mask;
        /* 'ownership' of prog_array is claimed by the first program that
         * is going to use this map or by the first program which FD is stored
         * in the map to make sure that all callers and callees have the same
diff --git a/include/linux/bpf_verifier.h b/include/linux/bpf_verifier.h
index 4c4e935..070fc49 100644
--- a/include/linux/bpf_verifier.h
+++ b/include/linux/bpf_verifier.h
@@ -67,7 +67,10 @@ struct bpf_verifier_state_list {
 };
 
 struct bpf_insn_aux_data {
-       enum bpf_reg_type ptr_type;     /* pointer type for load/store insns */
+       union {
+               enum bpf_reg_type ptr_type;     /* pointer type for load/store insns */
+               struct bpf_map *map_ptr;        /* pointer for call insn into lookup_elem */
+       };
        bool seen; /* this insn was processed by the verifier */
 };
 
diff --git a/kernel/bpf/arraymap.c b/kernel/bpf/arraymap.c
index f3721e1..bc57ead 100644
--- a/kernel/bpf/arraymap.c
+++ b/kernel/bpf/arraymap.c
@@ -46,9 +46,10 @@ static int bpf_array_alloc_percpu(struct bpf_array *array)
 static struct bpf_map *array_map_alloc(union bpf_attr *attr)
 {
        bool percpu = attr->map_type == BPF_MAP_TYPE_PERCPU_ARRAY;
+       u32 elem_size, index_mask, max_entries;
+       bool unpriv = !capable(CAP_SYS_ADMIN);
        struct bpf_array *array;
        u64 array_size;
-       u32 elem_size;
 
        /* check sanity of attributes */
        if (attr->max_entries == 0 || attr->key_size != 4 ||
@@ -63,11 +64,20 @@ static struct bpf_map *array_map_alloc(union bpf_attr *attr)
 
        elem_size = round_up(attr->value_size, 8);
 
+       max_entries = attr->max_entries;
+       index_mask = roundup_pow_of_two(max_entries) - 1;
+
+       if (unpriv)
+               /* round up array size to nearest power of 2,
+                * since cpu will speculate within index_mask limits
+                */
+               max_entries = index_mask + 1;
+
        array_size = sizeof(*array);
        if (percpu)
-               array_size += (u64) attr->max_entries * sizeof(void *);
+               array_size += (u64) max_entries * sizeof(void *);
        else
-               array_size += (u64) attr->max_entries * elem_size;
+               array_size += (u64) max_entries * elem_size;
 
        /* make sure there is no u32 overflow later in round_up() */
        if (array_size >= U32_MAX - PAGE_SIZE)
@@ -77,6 +87,8 @@ static struct bpf_map *array_map_alloc(union bpf_attr *attr)
        array = bpf_map_area_alloc(array_size);
        if (!array)
                return ERR_PTR(-ENOMEM);
+       array->index_mask = index_mask;
+       array->map.unpriv_array = unpriv;
 
        /* copy mandatory map attributes */
        array->map.map_type = attr->map_type;
@@ -110,7 +122,7 @@ static void *array_map_lookup_elem(struct bpf_map *map, void *key)
        if (unlikely(index >= array->map.max_entries))
                return NULL;
 
-       return array->value + array->elem_size * index;
+       return array->value + array->elem_size * (index & array->index_mask);
 }
 
 /* Called from eBPF program */
@@ -122,7 +134,7 @@ static void *percpu_array_map_lookup_elem(struct bpf_map *map, void *key)
        if (unlikely(index >= array->map.max_entries))
                return NULL;
 
-       return this_cpu_ptr(array->pptrs[index]);
+       return this_cpu_ptr(array->pptrs[index & array->index_mask]);
 }
 
 int bpf_percpu_array_copy(struct bpf_map *map, void *key, void *value)
@@ -142,7 +154,7 @@ int bpf_percpu_array_copy(struct bpf_map *map, void *key, void *value)
         */
        size = round_up(map->value_size, 8);
        rcu_read_lock();
-       pptr = array->pptrs[index];
+       pptr = array->pptrs[index & array->index_mask];
        for_each_possible_cpu(cpu) {
                bpf_long_memcpy(value + off, per_cpu_ptr(pptr, cpu), size);
                off += size;
@@ -190,10 +202,11 @@ static int array_map_update_elem(struct bpf_map *map, void *key, void *value,
                return -EEXIST;
 
        if (array->map.map_type == BPF_MAP_TYPE_PERCPU_ARRAY)
-               memcpy(this_cpu_ptr(array->pptrs[index]),
+               memcpy(this_cpu_ptr(array->pptrs[index & array->index_mask]),
                       value, map->value_size);
        else
-               memcpy(array->value + array->elem_size * index,
+               memcpy(array->value +
+                      array->elem_size * (index & array->index_mask),
                       value, map->value_size);
        return 0;
 }
@@ -227,7 +240,7 @@ int bpf_percpu_array_update(struct bpf_map *map, void *key, void *value,
         */
        size = round_up(map->value_size, 8);
        rcu_read_lock();
-       pptr = array->pptrs[index];
+       pptr = array->pptrs[index & array->index_mask];
        for_each_possible_cpu(cpu) {
                bpf_long_memcpy(per_cpu_ptr(pptr, cpu), value + off, size);
                off += size;
diff --git a/kernel/bpf/verifier.c b/kernel/bpf/verifier.c
index 2737041..19c44cf 100644
--- a/kernel/bpf/verifier.c
+++ b/kernel/bpf/verifier.c
@@ -1187,7 +1187,7 @@ static void clear_all_pkt_pointers(struct bpf_verifier_env *env)
        }
 }
 
-static int check_call(struct bpf_verifier_env *env, int func_id)
+static int check_call(struct bpf_verifier_env *env, int func_id, int insn_idx)
 {
        struct bpf_verifier_state *state = &env->cur_state;
        const struct bpf_func_proto *fn = NULL;
@@ -1238,6 +1238,13 @@ static int check_call(struct bpf_verifier_env *env, int func_id)
        err = check_func_arg(env, BPF_REG_2, fn->arg2_type, &meta);
        if (err)
                return err;
+       if (func_id == BPF_FUNC_tail_call) {
+               if (meta.map_ptr == NULL) {
+                       verbose("verifier bug\n");
+                       return -EINVAL;
+               }
+               env->insn_aux_data[insn_idx].map_ptr = meta.map_ptr;
+       }
        err = check_func_arg(env, BPF_REG_3, fn->arg3_type, &meta);
        if (err)
                return err;
@@ -3019,7 +3026,7 @@ static int do_check(struct bpf_verifier_env *env)
                                        return -EINVAL;
                                }
 
-                               err = check_call(env, insn->imm);
+                               err = check_call(env, insn->imm, insn_idx);
                                if (err)
                                        return err;
 
@@ -3372,7 +3379,11 @@ static int fixup_bpf_calls(struct bpf_verifier_env *env)
        struct bpf_insn *insn = prog->insnsi;
        const struct bpf_func_proto *fn;
        const int insn_cnt = prog->len;
-       int i;
+       struct bpf_insn insn_buf[16];
+       struct bpf_prog *new_prog;
+       struct bpf_map *map_ptr;
+       int i, cnt, delta = 0;
+
 
        for (i = 0; i < insn_cnt; i++, insn++) {
                if (insn->code != (BPF_JMP | BPF_CALL))
@@ -3390,6 +3401,31 @@ static int fixup_bpf_calls(struct bpf_verifier_env *env)
                         */
                        insn->imm = 0;
                        insn->code |= BPF_X;
+
+                       /* instead of changing every JIT dealing with tail_call
+                        * emit two extra insns:
+                        * if (index >= max_entries) goto out;
+                        * index &= array->index_mask;
+                        * to avoid out-of-bounds cpu speculation
+                        */
+                       map_ptr = env->insn_aux_data[i + delta].map_ptr;
+                       if (!map_ptr->unpriv_array)
+                               continue;
+                       insn_buf[0] = BPF_JMP_IMM(BPF_JGE, BPF_REG_3,
+                                                 map_ptr->max_entries, 2);
+                       insn_buf[1] = BPF_ALU32_IMM(BPF_AND, BPF_REG_3,
+                                                   container_of(map_ptr,
+                                                                struct bpf_array,
+                                                                map)->index_mask);
+                       insn_buf[2] = *insn;
+                       cnt = 3;
+                       new_prog = bpf_patch_insn_data(env, i + delta, insn_buf, cnt);
+                       if (!new_prog)
+                               return -ENOMEM;
+
+                       delta    += cnt - 1;
+                       env->prog = prog = new_prog;
+                       insn      = new_prog->insnsi + i + delta;
                        continue;
                }
 
(END)

Thanks & Regards

Rahul Kumar