Currently I use a AM335x in a project, in which we have planned to use two Ethernet ports in RMII-mode, i.e. rmii1 and rmii2.
RMII-1 functions correctly, but regarding RMII-2 only works the transmit part. I can't receive anything on RMII-2. The LAN chip
is LAN8710. I can see on the oscilloscope that the RMII-2 port on sitara is fed mit receiving signal, but absolutely no trace of receive.
I have also investigated the values of different registers, e.g. statistics, Ethernet-RAM, etc, but unfortunately nothing is seen
with regard to receiving. I would like to know, if it is possible to use simultaneously two ethernet ports on AM3358 in RMII-mode?