Part Number: TMS320C5517
Other Parts Discussed in Thread: TMS320C5505
Hi everyone,
I have designed the hardware using mentioned TI DSP. The first release of the hardware has included USB peripheral and all components that are related was populated on board. Originally we have planned to use the USB for the communication, but after some discussion and first release, we figured out that there is no need for this peripheral at all. Currently, I am trying to optimize the cost and since the USB is not needed at all I would like to exclude all components and make it NI. This should be done without changing the PCB design and I have some concerns that are listed below:
- Is it ok to leave USB_MXI, USB_MXO, and USB_VSSOSC unconnected?
- Is it ok to leave USB_R1 and USB_VSSREF connected with the 10k resistor? There is no way to connect USB_VSSREF to the ground, it's not possible on the current design.
- Is it ok to leave USB_DM and USB_DP unconnected?
- Is it ok to leave USB_VBUS unconnected?
Rest of the pins that are related to the USB peripheral will be connected as has been proposed in the DSP datasheet
USB_VDDA3P3 -> GND
USB_VDDA1P3 -> GND
USB_VDD1P3 -> GND
USB_VDDPLL -> GND
USB_VDDOSC -> GND
Thanks in advance, best regards.