Hello.
With the AM5716, is there a way to adjust the drive strength of a specific pin? We can adjust for the SDRAM pins and the MMC1 pins only, but with others pins? Like the UART pins...
We have an overshoot and undershoot issue with some pins, since those pin drive too high the output.
There is a register to set the slew rate, but there is not much effect on the signal integrity (ex.: bit19, UART2_RTSN_SLEWCONTROL)
Regards.