Other Parts Discussed in Thread: AM3352
Hello,
We would like to build a system offloading an EtherCAT master to a Sitara, connecting it to the main processor using two USB connections (one for data up and one for data down stream) and 2 ethernet ports.
From this thread i learned that EtherCAT Master does not require the PRU unit but may use any ethernet interface. It also states that there is no EtherCAT master stack/software/example available from TI, however this information is >6 years old and i found information on an acontis based TI stack.
- Is there an EtherCAT master library available from TI? (even if some porting is needed)
- bare metal or linux?
- Are bare metal USB stacks available from TI?
- The AM335x series is a bit older by now, how long will they be available at least? (especially the AM3352)
- Would you suggest to add additional RAM for 2xETH + EtherCAT stack & 2xUSB + stacks?
Thank you,
Regards,
Lars