This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCI6630K2L: K2L DDR3 reset issue

Part Number: TCI6630K2L

Hello,

We are using K2L EVM design for one of our enodeB design.

Currently we are testing the Board. The K2L is reset signal, POR signal are OK, we are able to see communicate in the serial console and start Uboot. but when DDR3 init is started, the DDR3 Reset is driven low and remains low, it is not going High. Not sure if the K2L DDR3 controller is working. The DDR clock (100MHz) input to K2L is OK. Kindly advice whether the K2L Processor need to be replaced? Or is there any way to confirm the chip is OK?

Regards,

Sumathi