A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
which DSP is suitable to control 2 phase planar motor?
All C2000 devices can control such a two-phase motor with a right gate drive and power modular. We didn't have any example library to control a two-phase planar motor, but you might refer to the example project for a stepper motor in controlSUITE as the following folder that should be similar to your requirement.
C:\ti\controlSUITE\development_kits\DRV8412-C2-KIT_v131\Stepper