Part Number: AM4378
I am using the spreadsheet to figure out the values and i am at the point of including the trace lengths for the board. i am reading
to understand the details. i have 2 questions about this
1) we have 2 16 bit DDR3 chips attached to the ARM to make it 32 bits. is the trace length meant to be the total trace for the memory? so for example if chip 1 is 1 inch away and chip 2 is 1.5 inches away (.5 inches from chip 1) my lengths would be 1 inch for byte 1 and 2 and 1.5 inches for bytes 3 and 4, correct?
2) is there a DDR leveling procedure that i have to do the first time powering up the board or is that all handled by linux during boot up?