Part Number: AM5728
Tool/software: Linux
Hi,
I m using yocto processor-sdk-04.02.00.09. I have tried to enable the USB OTG in custom board.
root@am57xx-evm:~# dmesg | grep "usb"
[ 3.562032] ldousb: disabling
[ 7.263711] palmas-usb 48070000.i2c:tps659038@58:tps659038_usb: GPIO lookup for consumer id
[ 7.263717] palmas-usb 48070000.i2c:tps659038@58:tps659038_usb: using device tree for GPIO lookup
[ 7.263723] of_get_named_gpiod_flags: can't parse 'id-gpios' property of node '/ocp/i2c@48070000/tps659038@58/tps659038_usb[0]'
[ 7.263728] of_get_named_gpiod_flags: can't parse 'id-gpio' property of node '/ocp/i2c@48070000/tps659038@58/tps659038_usb[0]'
[ 7.263736] palmas-usb 48070000.i2c:tps659038@58:tps659038_usb: using lookup tables for GPIO lookup
[ 7.263747] palmas-usb 48070000.i2c:tps659038@58:tps659038_usb: lookup for GPIO id failed
[ 7.263753] palmas-usb 48070000.i2c:tps659038@58:tps659038_usb: GPIO lookup for consumer vbus
[ 7.263757] palmas-usb 48070000.i2c:tps659038@58:tps659038_usb: using device tree for GPIO lookup
[ 7.263762] of_get_named_gpiod_flags: can't parse 'vbus-gpios' property of node '/ocp/i2c@48070000/tps659038@58/tps659038_usb[0]'
[ 7.263833] of_get_named_gpiod_flags: parsed 'vbus-gpio' property of node '/ocp/i2c@48070000/tps659038@58/tps659038_usb[0]' - status (0)
[ 8.513524] usbcore: registered new interface driver usbfs
[ 8.513691] usbcore: registered new interface driver hub
[ 8.513864] usbcore: registered new device driver usb
[ 8.547381] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
root@am57xx-evm:~#
root@am57xx-evm:~#
root@am57xx-evm:~# lsusb
Bus 002 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
root@am57xx-evm:~#
USB 1 port is working with default configuration.
usb2 is configured in DTS as follows :
&usb2_phy1 {
phy-supply = <&ldousb_reg>;
};
&usb2_phy2 {
phy-supply = <&ldousb_reg>;
};
&usb1 {
dr_mode = "host";
};
&omap_dwc3_2 {
extcon = <&extcon_usb2>;
};
&usb2 {
/*
* Stand alone usage is peripheral only.
* However, with some resistor modifications
* this port can be used via expansion connectors
* as "host" or "dual-role". If so, provide
* the necessary dr_mode override in the expansion
* board's DT.
*/
dr_mode = "peripheral";
};
In Menuconfig I have added the below supports :
+CONFIG_USB_DYNAMIC_MINORS=y
+CONFIG_USB_OTG=y
+CONFIG_USB_OTG_WHITELIST=y
+CONFIG_USB_OTG_FSM=m
+CONFIG_USB_GADGET_DEBUG=y
+# CONFIG_USB_GADGET_VERBOSE is not set
+# CONFIG_USB_ZERO_HNPTEST is not set
There is no voltage in USB2_5V pin.
Please provide the Guidance to Enable USB2 as OTG (MICRO USB TYPE B FEMALE connector)