Part Number: AM3352
Tool/software: Linux
Hi,
We are facing a driver crash when trying to use openssl.. Below is the crash dump (similar to the one reported in the link
)
Kernel version: 4.9.69
1568.755634] [<c010b790>] (dump_backtrace) from [<c010ba4c>] (show_stack+0x18/0x1c)
[ 1568.773111] r7:00000009 r6:00000000 r5:c099c168 r4:00000000
[ 1568.778888] [<c010ba34>] (show_stack) from [<c03c1cd4>] (dump_stack+0x24/0x28)
[ 1568.801547] [<c03c1cb0>] (dump_stack) from [<c012b5a8>] (__warn+0xe8/0x100)
[ 1568.815231] [<c012b4c0>] (__warn) from [<c012b678>] (warn_slowpath_null+0x28/0x30)
[ 1568.831445] r9:064c10e0 r8:0000000f r7:00000000 r6:c0c13e00 r5:00000000 r4:c0c029c4
[ 1568.843271] [<c012b650>] (warn_slowpath_null) from [<c01c3cf8>] (__alloc_pages_nodemask+0x804/0xbdc)
[ 1568.852498] [<c01c34f4>] (__alloc_pages_nodemask) from [<c01c40e8>] (__get_free_pages+0x18/0x34)
[ 1568.866397] r10:00000000 r9:064c10e0 r8:ca2f6000 r7:00000040 r6:c0080000 r5:cf691710
[ 1568.880361] r4:cf7a3e00
[ 1568.886667] [<c01c40d0>] (__get_free_pages) from [<bf086138>] (omap_sham_handle_queue+0x558/0x9dc [omap_sham])
[ 1568.900624] [<bf085be0>] (omap_sham_handle_queue [omap_sham]) from [<bf086760>] (omap_sham_update+0x68/0xa8 [omap_sham])
[ 1568.915606] r10:00000000 r9:ca2f6000 r8:becac134 r7:c0080000 r6:00000000 r5:ca078d80
[ 1568.927485] r4:cf7a3e00
[ 1568.930197] [<bf0866f8>] (omap_sham_update [omap_sham]) from [<bf003494>] (cryptodev_hash_update+0x40/0xcc [cryptodev])
[ 1568.945936] r5:ca078d80 r4:ca078dd0
[ 1568.949686] [<bf003454>] (cryptodev_hash_update [cryptodev]) from [<bf001f90>] (hash_n_crypt+0xe4/0x140 [cryptodev])
[ 1568.969536] r4:ca078d80
[ 1568.972242] [<bf001eac>] (hash_n_crypt [cryptodev]) from [<bf0024e4>] (crypto_run+0x204/0x4f4 [cryptodev])
[ 1568.986859] r7:ca2f7dcc r6:c8a4e700 r5:ca078d80 r4:ca2f7dcc
[ 1568.992696] [<bf0022e0>] (crypto_run [cryptodev]) from [<bf0018e4>] (cryptodev_ioctl+0x424/0x9ec [cryptodev])
[ 1569.011783] r8:becac134 r7:ca2f7dcc r6:c8a96200 r5:becac134 r4:00000051
[ 1569.022430] [<bf0014c0>] (cryptodev_ioctl [cryptodev]) from [<c0225b68>] (do_vfs_ioctl+0xa8/0x980)
[ 1569.035511] r9:ca2f6000 r8:becac134 r7:00000003 r6:cf690a80 r5:cf572898 r4:becac134
[ 1569.047306] [<c0225ac0>] (do_vfs_ioctl) from [<c022647c>] (SyS_ioctl+0x3c/0x64)
[ 1569.058436] r10:00000000 r9:ca2f6000 r8:becac134 r7:c01c6368 r6:cf690a80 r5:00000003
[ 1569.070028] r4:cf690a80
[ 1569.072661] [<c0226440>] (SyS_ioctl) from [<c0107c80>] (ret_fast_syscall+0x0/0x48)
[ 1569.085285] r9:ca2f6000 r8:c0107e44 r7:00000036 r6:d734a3eb r5:064c10e0 r4:00000000
[ 1569.099025] ---[ end trace f92bc7a3f3a124ee ]---
[ 1569.107484] omap_sham_copy_sgs: Couldn't allocate pages for unaligned cases.
[ 1569.118560] cryptodev: openssl[1281] (waitfor:267): error from async request: -12
[ 1569.129993] cryptodev: openssl[1281] (hash_n_crypt:98): CryptoAPI failure: -12
Verification failure
Is there a fix for this issue available as a patch that we can download and apply?
Regards,
Fariya