This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM355(DM365) interface with CCD sensor



Hi,all

    If the VPFE interface with CCD sensor (not CMOS sensor) in DM355(365), Do a  CPLD IC must be used  to provide CCD control signal?

also the onfiguring of CCD +TG+AFE+DM355(365)  is ok or not?   

  DO the DVEVM365(355)  provide the examle of VPFE interfaced with CCD sensor?

   Thank you very much!

   Jonson.huang