This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm355 ECC error while reading bad block table



hi all

Today,I updata the dvsdk to 2.0

I use legacy mode for my nand flash

NAND_programmer_legacy.out    - Flash writer (CCS application) for NAND flash
u-boot-1.2.0-dm355-legacy.bin    - U-Boot for NAND flash
uImage-dm355-legacy        - Linux kernel Image
ublDM355-nand-legacy.bin    - User Boot loader for NAND mode

I got a  "ECC error while reading bad block table" why?

The file " uImage-dm355-legacy "  be renamed to "uImage"

sysytem boot log:

UBL: Entering UBL NANDBoot routine
UBL:  NANDInit() Successful
UBL:  Nand Detected:  Manufacturers ID:  0x0000002C
UBL:                  Device ID:         0x000000D3
UBL:                  page size:         0x00000800 bytes per page
UBL:                  block size:         0x00000040 pages per block
UBL:                  address cycles:    00000005 cycles
UBL: detected valid U-Boot magic number
UBL: booting to U-Boot
 
 
U-Boot 1.2.0 (Mar 13 2009 - 12:24:35)
 
DRAM:  128 MB
NAND:  NAND device: Manufacturer ID: 0x2c, Chip ID: 0xd3 (Micron NAND 1GiB 3,3V 8-bit)
Bad block table found at page 524224, version 0x01
Bad block table found at page 524160, version 0x01
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xd3 (Micron NAND 1GiB 3,3V 8-bit)
Bad block table found at page 524224, version 0x01
Bad block table found at page 524160, version 0x01
2048 MiB
In:    serial
Out:   serial
Err:   serial
ARM Clock :- 216MHz
DDR Clock :- 171MHz
Hit any key to stop autoboot:  0  
DM355 EVM # tftp
TFTP from server 192.168.100.54; our IP address is 192.168.100.252
Filename 'uImage'.
Load address: 0x80700000
Loading: #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         ############################################################
done
Bytes transferred = 1970820 (1e1284 hex)
DM355 EVM # bootm
## Booting image at 80700000 ...
   Image Name:   Linux-2.6.18_pro500-davinci_evm-
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    1970756 Bytes =  1.9 MB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
OK
 
Starting kernel ...
 
Uncompressing Linux................................................................................................................................... done, booting the kernel.
Linux version 2.6.18_pro500-davinci_evm-arm_v5t_le (a0869522@gt906xs11.gt.design.ti.com) (gcc version 4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 PREEMPT Wed Mar 11 10:23:58 EDT 2009
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
Machine: DaVinci DM355 EVM
Memory policy: ECC disabled, Data cache writeback
DaVinci DM0350 variant 0x0
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Built 1 zonelists.  Total pages: 30720
Kernel command line: ip=dhcp mem=120M console=ttyS0,115200n8 root=/dev/ram0 rw initrd=0x82000000,4M
PID hash table entries: 512 (order: 9, 2048 bytes)
Clock event device timer0_0 configured with caps set: 03
Console: colour dummy device 80x30
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 120MB = 120MB total
Memory: 113280KB available (3397K code, 680K data, 168K init)
Security Framework v1.0.0 initialized
Capability LSM initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
checking if image is initramfs...it isn't (bad gzip magic numbers); looks like an initrd
Freeing initrd memory: 4096K
NET: Registered protocol family 16
DaVinci: 104 gpio irqs
ch0 default output "COMPOSITE", mode "NTSC"
VPBE Encoder Initialized
LogicPD encoder initialized
SCSI subsystem initialized
usbcore: registered new driver usbfs
usbcore: registered new driver hub
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 4096 bind 2048)
TCP reno registered
VFS: Disk quotas dquot_6.5.1
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
squashfs: version 3.1 (2006/08/19) Phillip Lougher
JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.
yaffs Mar 11 2009 10:16:27 Installing.  
SGI XFS with no debug enabled
Initializing Cryptographic API
io scheduler noop registered
io scheduler anticipatory registered (default)
LTT : ltt-facilities init
LTT : ltt-facility-core init in kernel
davincifb davincifb.0: dm_osd0_fb: 720x480x16@0,0 with framebuffer size 1350KB
davincifb davincifb.0: dm_vid0_fb: 0x0x16@0,0 with framebuffer size 675KB
davincifb davincifb.0: dm_osd1_fb: 720x480x4@0,0 with framebuffer size 1350KB
davincifb davincifb.0: dm_vid1_fb: 0x0x16@0,0 with framebuffer size 675KB
DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfec20000 (irq = 40) is a 16550A
serial8250.0: ttyS1 at MMIO map 0x1c20400 mem 0xfec20400 (irq = 41) is a 16550A
serial8250 serial8250.0: unable to register port at index 2 (IO0 MEM1e06000 IRQ14): -28
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
dm9000 Ethernet Driver
eth0: dm9000 at c805e000,c8060002 IRQ 45 MAC: 00:0e:99:02:c3:26
netconsole: not configured, aborting
Linux video capture interface: v2.00
vpfe vpfe.1: DaVinci v4l2 capture driver V1.0 loaded
Trying to register davinci display video device.
layer=c70eb800,layer->video_dev=c70eb960
Trying to register davinci display video device.
layer=c70eb600,layer->video_dev=c70eb760
davinci_init:DaVinci V4L2 Display Driver V1.0 loaded
ipipe major#: 254, minor# 0
ipipe driver registered
af major#: 253, minor# 0
aew major#: 252, minor# 0
i2c /dev entries driver
nand_davinci nand_davinci.0: Using 4-bit hardware ECC
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xd3 (Micron NAND 1GiB 3,3V 8-bit)
2 NAND chips detected
nand_davinci_4bit_compare_ecc Too many errors to be corrected!
nand_davinci_4bit_compare_ecc Too many errors to be corrected!
nand_davinci_4bit_compare_ecc Too many errors to be corrected!
nand_davinci_4bit_compare_ecc Too many errors to be corrected!
nand_bbt: ECC error while reading bad block table
nand_davinci_4bit_compare_ecc Too many errors to be corrected!
nand_davinci_4bit_compare_ecc Too many errors to be corrected!
nand_davinci_4bit_compare_ecc Too many errors to be corrected!
nand_davinci_4bit_compare_ecc Too many errors to be corrected!

nand_bbt: ECC error while reading bad block table
Creating 5 MTD partitions on "nand_davinci.0":
0x00000000-0x003c0000 : "bootloader"
0x003c0000-0x00400000 : "params"
0x00400000-0x00800000 : "kernel"
0x00800000-0x20800000 : "filesystem1"
0x20800000-0x80000000 : "filesystem2"
nand_davinci nand_davinci.0: hardware revision: 2.3
dm_spi.0: davinci SPI Controller driver at 0xc8064000 (irq = 42) use_dma=0
Initializing USB Mass Storage driver...
usbcore: registered new driver usb-storage
USB Mass Storage support registered.
usbcore: registered new driver usbhid
drivers/usb/input/hid-core.c: v2.6:USB HID core driver
musb_hdrc: version 6.0, cppi-dma, host, debug=0
musb_hdrc musb_hdrc: No DMA interrupt line
musb_hdrc: USB Host mode controller at c8066000 using DMA, IRQ 12
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
usb usb1: configuration #1 chosen from 1 choice
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mice: PS/2 mouse device common for all mice
davinci-mmc davinci-mmc.0: Supporting 4-bit mode
davinci-mmc davinci-mmc.0: Using DMA mode
davinci-mmc davinci-mmc.1: Supporting 4-bit mode
davinci-mmc davinci-mmc.1: Using DMA mode
Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).
ASoC version 0.13.1
AIC3X Audio Codec 0.1
asoc: aic3x <-> davinci-i2s mapping ok
ALSA device list:
  #0: DaVinci DM355 EVM (aic3x)
IPv4 over IPv4 tunneling driver
TCP bic registered
NET: Registered protocol family 1
NET: Registered protocol family 17
Time: timer0_1 clocksource has been installed.
Clock event device timer0_0 configured with caps set: 08
Switched to high resolution mode on CPU 0
eth0: link down
Sending DHCP requests .<6>eth0: link up, 100Mbps, full-duplex, lpa 0x45E1