Hi, Is it possible to adjust GPIO drive strenght? I only found minimum 6mA mentioned on datasheet and other documents. If yes, what's the maximum?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The drive strength is not configurable. The specifications listed are those that are guaranteed. This device has a guaranteed minimum 6ma drive while driving high at a minimum voltage of VDDS-0.45V or while driving low at a maximum voltage of 0.45V. If you need to drive high current loads, we can recommend driver devices that are appropriate at:
We also have specialty drivers available that we can help you locate.
Tom