The DDR3 maximum frequency for industrial extended temperature is shown in Table 5-6 on AM335x datasheet (SPRS717K).
I understand that the DDR3 maximum frequency when VDD_CORE is OPP100 is as follows.
-40°C to 105°C : 400 MHz
105°C to 125°C : 333 MHz
Is my understanding correct?
Best regards,
Daisuke