Tool/software: Code Composer Studio
I post this issue in this forum because I don't know where else to post, sorry.
---
I have a AM6548-IDK and a small program for the A53 core.
Here I have the following 2 lines of code:
UART_printf("d: %d\n", 100000);
App_print( "d: %d\n", 100000);
Here is the function App_print() :
void App_print(const char *format, ...)
{
va_list vaArgPtr;
va_start(vaArgPtr, format);
UART_printf(format, vaArgPtr);
va_end(vaArgPtr);
}
Now the vaargs in the App_print don't work, the forwarding of the variable arguments don't work.
The UART output is:
d: 100000
d: 1879506800
Up to now I spend a full day on this doing a lot of double-checks, vsnprintf, checking compiler options, searching gcc bugs via google etc.
Has anyone an idea?
Ruediger