Tool/software: Linux
Hi Sir,
My HW is TDA2x CPU board + Vision Board + daughter board + LVDS sensor and SDK is PROCESSOR_SDK_VISION_03_04_00_00 with TDA2XX_EVM_LINUX_ALL define.
I select use-case "4CH VIP LVDS capture + SGX MOSAIC + DISPLAY".
I want to save the source image in this ues-case, then I add some function code in this case (chains_lvdsVipMultiCam_SgxDisplay.c),
example "static Void mountFatFs()", "static Void saveCaptureFrames(chains_srvCalibration_DisplayAppObj *pObj)"....etc.
After boot on the EVK and select this use-case, it can't be executed successfully, console mode shows below error message:
****** Segmentation fault caught ....
Faulty address is 0x4, called from 0x1b155
Totally Obtained 0 stack frames. signal number =11
Signal number = 11, Signal errno = 0
SI code = 1 (Address not mapped to object)
Fault addr = 0x4
[bt] Execution path:
root@dra7xx-evm:/opt/vision_sdk#
What does it mean?
Please help and thanks.
Ranny.