Other Parts Discussed in Thread: MAX3221
I was running through the Software Setup in UBuntu guide 2 weeks ago and had mounted the file system on an uBuntu host PC and successfully booted up using the NFS server. I had successfully compiled the "Hello World" app on the host PC and run the app on the target DVEVM (Rev C). Everything was going great. I was then forced to put the development on hold to complete another project. I have finally completed the previous project and have now finally pulled out the DVEVM out again to continue the development.
I am however now unable to get any comms coming out the board - no console interface - nothing (well except the single 0x00 I get when I plug in the power... ). I have tested the RX portion of the MAX3221 IC and the DM265 is definitely receiving comms from Window Hyperterminal (@115200, 8N1). This puts my mind at ease with regard to my USB - Serial converter. There is however definitely nothing coming from the DM365 into even the DVEVMS MAX3221. Ie it appears the DM365 is not transmitting anything. Remembering that I did save the new environment variables I am now wondering about what happens if the DVEVM does not find the host PC upon bootup? We are running a DHCP server at work so I am doubtful that it is on the same IP.
My question is thus as follows, should I be seeing anything from the DB9 even if the DM365 cannot find the NFS server? Surely I will still see some uBoot output?
If I should be seeing some comms, I am concerned - should the next logical thought be that something has gone wrong with the HW? The DVEVM accompanied me home a number of times (protected) during
optimistic weekends when I was hoping to get a chance to continue
playing. I am now forced to consider whether it may have been damaged. How could I test this? What is my next "best bet" step?
I am very new to both Linux and the DaVinci family so I was feeling my way with the Software Guide, learning as I went. I am planning to rerun through all the steps in the "Software Setup in Ubuntu" guide to see if I can make a difference. Any input or ideas on what has happened would be appreciated. Thanks.
NickA