This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320DM6446: SDXC of SD card support

Part Number: TMS320DM6446

Hi,

Does TMS320DM6446 support SDXC of SD card?

It seems to support SDHC.

http://processors.wiki.ti.com/index.php/Managed_NAND

We think the electrical specs of SDHC and SDXC are similar and the difference is file system (FAT32 and exFAT).

Best Regards,

  • Hi Masashi,

    It seems to me that DM644x device do NOT support SDXC. This is what we have in DM644x MMC/SD user guide:

    www.ti.com/.../sprue30d.pdf

    1.2 Features
    The MMC/SD card controller has the following features:
    25 MHZ maximum clock to SD (specification version 1.1)
    Supports SDHC
    The MMC/SD Controller supports SDHC address range but is limited to the 25MHz memory card clock.

    1.5 Industry Standard(s) Compliance Statement
    The MMC/SD card controller supports the following industry standards (with the exception noted below):
    SD (Secure Digital) Physical Layer Specification V1.1

    SDXC is defined in version 3.01 of the SD specification, while DM644x MMC/SD controller support v1.1

    Regards,
    Pavel
  • Hi Pavel-san,

    Thank for your quick response and explanation in detail.
    I understood.

    Best Regards,
    Masashi