This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS: [SDK_03_06][TDA3x][AWR1243] Booting problem.



Tool/software: TI-RTOS

Hi

I'm using TDA3xx EVM, PROCESSOR RADAR SDK_03_06 version.

and mmwave_dfp_01_02_00_00 version of AWR1243.

when i would like to boot radar board, error log happened below Utils_dspExceptionHookFxn:.

i don't know what those mean below Utils_dspExceptionHookFxn:.

i need your help.

[IPU1-0] 7.502989 s: CHAINS: Init AR12xx ... DONE !!!
[IPU1-0] 7.503812 s: ISSCAPTURE: Create in progress !!!
[IPU1-0] 7.525010 s: ISSCAPTURE: Create Done !!!
[IPU1-0] 7.525254 s: IPC_OUT_0 : Create in progress !!!
[IPU1-0] 7.525559 s: IPC_OUT_0 : Create Done !!!
[IPU1-0] 7.534648 s: IPC_IN_0 : Create in progress !!!
[IPU1-0] 7.535411 s: IPC_IN_0 : Create Done !!!
[IPU1-0] 7.535624 s: DISPLAY: Create in progress !!!
[IPU1-0] 7.536082 s: DISPLAY: Create Done !!!
[IPU1-0] 7.536295 s: GRPXSRC: Create in progress !!!
[IPU1-0] 7.712346 s: GRPXSRC: Create Done !!!
[IPU1-0] 7.712712 s: DISPLAY: Create in progress !!!
[IPU1-0] 7.713139 s: DISPLAY: Create Done !!!
[IPU1-0] 7.713261 s: SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1023
[IPU1-0] 7.713353 s: SYSTEM: Heap = LOCAL_DDR @ 0x00000000, Total size = 262144 B (256 KB), Free size = 258288 B (252 KB)
[IPU1-0] 7.713505 s: SYSTEM: Heap = SR_OCMC @ 0x00000000, Total size = 0 B (0 KB), Free size = 0 B (0 KB)
[IPU1-0] 7.713688 s: SYSTEM: Heap = SR_DDR_CACHED @ 0x82f7fc00, Total size = 77594624 B (74 MB), Free size = 71874560 B (68 MB)
[IPU1-0] 7.713841 s: SYSTEM: Heap = SR_DDR_NON_CACHED @ 0x00000000, Total size = 0 B (0 MB), Free size = 0 B (0 MB)
[IPU1-0] 7.718782 s: DISPLAY: Start in progress !!!
[IPU1-0] 7.718873 s: DISPLAY: Start Done !!!
[IPU1-0] 7.721740 s: DISPLAY: Start in progress !!!
[IPU1-0] 7.721832 s: DISPLAY: Start Done !!!
[IPU1-0] 7.722137 s: ISSCAPTURE: Start in progress !!!
[IPU1-0] 7.722259 s: ISSCAPTURE: Start Done !!!
[IPU1-0] 7.722351 s: CHAINS: AR12xx Starting Radar Sensor ...
[IPU1-0] 7.725523 s: CHAINS: AR12xx Starting Radar Sensor ... DONE !!!
[IPU1-0] 7.726163 s:
[IPU1-0]
[IPU1-0] ====================
[IPU1-0] Chains Run-time Menu
[IPU1-0] ====================
[IPU1-0]
[IPU1-0] 0: Stop Chain
[IPU1-0]
[IPU1-0]
[IPU1-0] p: Print Performance Statistics
[IPU1-0]
[IPU1-0] Enter Choice:
[IPU1-0]
[IPU1-0] 7.726346 s:
[IPU1-0] Unsupported option ' '. Please try again
[IPU1-0] 7.726438 s:
[IPU1-0]
[IPU1-0] ====================
[IPU1-0] Chains Run-time Menu
[IPU1-0] ====================
[IPU1-0]
[IPU1-0] 0: Stop Chain
[IPU1-0]
[IPU1-0]
[IPU1-0] p: Print Performance Statistics
[IPU1-0]
[IPU1-0] Enter Choice:
[IPU1-0]
[IPU1-1] 7.714115 s: SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1023
[IPU1-1] 7.714237 s: SYSTEM: Heap = LOCAL_DDR @ 0x00000000, Total size = 262144 B (256 KB), Free size = 259640 B (253 KB)
[DSP1 ] 7.525742 s: IPC_IN_0 : Create in progress !!!
[DSP1 ] 7.526047 s: IPC_IN_0 : Create Done !!!
[DSP1 ] 7.526200 s: ALGORITHM: Create in progress (algId = 11) !!!
[DSP1 ] 7.529433 s: UTILS: DMA: Allocated CH (TCC) = 24 (24)
[DSP1 ] 7.529463 s: UTILS: DMA: 0 of 1: Allocated PaRAM = 24 (0x43305200)
[DSP1 ] 7.531141 s: ALG: TI.radar.zoomfft: CH0 BUF0: 0x83251400 ( 691200 B )
[DSP1 ] 7.532696 s: ALG: TI.radar.zoomfft: CH0 BUF1: 0x832fa000 ( 691200 B )
[DSP1 ] 7.534252 s: ALG: TI.radar.zoomfft: CH0 BUF2: 0x833a2c00 ( 691200 B )
[DSP1 ] 7.534313 s: ALGORITHM: Create Done (algId = 11) !!!
[DSP1 ] 7.534465 s: IPC_OUT_0 : Create in progress !!!
[DSP1 ] 7.534526 s: IPC_OUT_0 : Create Done !!!
[DSP1 ] 7.714481 s: SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1023
[DSP1 ] 7.714512 s: SYSTEM: Heap = LOCAL_L2 @ 0x00800000, Total size = 227264 B (221 KB), Free size = 227264 B (221 KB)
[DSP1 ] 7.714573 s: SYSTEM: Heap = LOCAL_DDR @ 0x00000000, Total size = 524288 B (512 KB), Free size = 501872 B (490 KB)
[DSP1 ] 7.865735 s: Measure Cfg: 0 434 512
[DSP1 ] 7.866619 s: FFT Windows is BLACKMAN_NUTTALL(third Order)!!
[EVE1 ] 7.714847 s: SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1023
[EVE1 ] 7.715701 s: SYSTEM: Heap = LOCAL_L2 @ 0x40020000, Total size = 22528 B (22 KB), Free size = 22528 B (22 KB)
[EVE1 ] 7.717226 s: SYSTEM: Heap = LOCAL_DDR @ 0x00000000, Total size = 262144 B (256 KB), Free size = 261800 B (255 KB)
[IPU1-0] 8.009607 s: Utils_dspExceptionHookFxn:
[IPU1-0] 8.009638 s: efr=0x2
[IPU1-0] 8.009638 s: nrp=0xe244008
[IPU1-0] 8.009668 s: ntsr=0x1820d
[IPU1-0] 8.009668 s: ierr=0x0
[IPU1-0] 8.009699 s: excContext=0x837e98
[IPU1-0] 8.009699 s: A0=0xd6b82ef0 A1=0x0
[IPU1-0] 8.009729 s: A2=0x0 A3=0xe44cb0b0
[IPU1-0] 8.009760 s: A4=0x69c5912f A5=0x41
[IPU1-0] 8.009760 s: A6=0x6b5c177 A7=0x3b3d
[IPU1-0] 8.009790 s: A8=0x0 A9=0x8294de54
[IPU1-0] 8.009790 s: A10=0x0 A11=0x2787
[IPU1-0] 8.009821 s: A12=0x10 A13=0x208b000
[IPU1-0] 8.009821 s: A14=0x0 A15=0x827dbddc
[IPU1-0] 8.009851 s: A16=0x3 A17=0x1
[IPU1-0] 8.009882 s: A18=0xd A19=0xc62d9c00
[IPU1-0] 8.009882 s: A20=0x0 A21=0x0
[IPU1-0] 8.009912 s: A22=0x81202220 A23=0x0
[IPU1-0] 8.009912 s: A24=0x8120d2ac A25=0x827dbdf4
[IPU1-0] 8.009943 s: A26=0x82943770 A27=0x82943780
[IPU1-0] 8.009973 s: A28=0x829458f8 A29=0x7
[IPU1-0] 8.009973 s: A30=0x20 A31=0xffffffff
[IPU1-0] 8.010004 s: B0=0xe24400b B1=0x1
[IPU1-0] 8.010004 s: B2=0x0 B3=0x81217900
[IPU1-0] 8.010034 s: B4=0x10 B5=0xa0
[IPU1-0] 8.010034 s: B6=0xe24400b B7=0x7ffffff
[IPU1-0] 8.010065 s: B8=0x400000 B9=0x0
[IPU1-0] 8.010095 s: B10=0x69c5912f B11=0xe24400b
[IPU1-0] 8.010095 s: B12=0x827db888 B13=0xe24400b
[IPU1-0] 8.010126 s: B14=0x82952038 B15=0x837cf0
[IPU1-0] 8.010126 s: B16=0x0 B17=0x41
[IPU1-0] 8.010156 s: B18=0x80000000 B19=0x530
[IPU1-0] 8.010187 s: B20=0x15000103 B21=0x8
[IPU1-0] 8.010187 s: B22=0x20f B23=0x0
[IPU1-0] 8.010217 s: B24=0x1ec023a0 B25=0x5440906c
[IPU1-0] 8.010217 s: B26=0x140005da B27=0x827dbb08
[IPU1-0] 8.010248 s: B28=0x82943798 B29=0x827dbde0
[IPU1-0] 8.010278 s: B30=0x71644bc0 B31=0x0
[IPU1-0] 8.010278 s: NTSR=0x1820d
[IPU1-0] 8.010309 s: ITSR=0x20d
[IPU1-0] 8.010309 s: IRP=0x81217702
[IPU1-0] 8.010339 s: SSR=0x0
[IPU1-0] 8.010339 s: AMR=0x0
[IPU1-0] 8.010370 s: RILC=0x0
[IPU1-0] 8.010370 s: ILC=0x0
[IPU1-0] 8.010400 s: Terminating Execution...
[IPU1-0] 8.010492 s:
[IPU1-0] 8.010492 s: ### XDC ASSERT - ERROR CALLBACK START ###
[IPU1-0] 8.010522 s:
[IPU1-0] 8.010583 s: E_exceptionMax: pc = 0x0e244008, sp = 0x00837cf0.
[IPU1-0] 8.010614 s:
[IPU1-0] 8.010614 s: ### XDC ASSERT - ERROR CALLBACK END ###
[IPU1-0] 8.010644 s: