Hello,
We have some questions about the relationship between DMA transfer and MPU-EMIF direct access on AM5748.
There are two DMA module, System DMA and Enhanced DMA, so could you confirm the following questions against each DMA?
1.While DMA is transferring data to DRAM, is A15 able to access DRAM directly (MPU -> EMIF -> SDRAM)?
In other words, is A15 able to interrupt the other module's transaction of DMA access?
2.In above case, is DMA able to suspend the processing transaction and release the bus (channel) resource?
3.If the answer of question 2 is yes, could you tell us the timing when the bus resource is released?
We want to know, for example, the timing is the end of block transfer, the end of burst transfer, or something.
Best Regards,
Nomo