This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5748: Exclusive operation of read and write transfer in DMA module on AM5748

Guru 16800 points
Part Number: AM5748


Hello,

Could you tell me the way to control DMA read transfer and write transfer exclusively?
There are two DMA module, System DMA and Enhanced DMA, so could you confirm the feasibility against each DMA?

In normal case, read transfer and write transfer work in parallel and the bus resource is occupied.
My customers want to avoid the situation.
So, they want to stop read transfer by the end of write transfer and stop write transfer by the end of read transfer.

Best Regards,
Nomo