Part Number: TDA2P-ACD
Hi Experts,
My customer tries to use Ethernet on TDA2Px RVP. But Ethernet doesn't work. They don't see "NDK: Link Status: 1000Mb/s Full Duplex on PHY 12". Also, if they ping from the machine, no response returned.
They are using Radar SDK 3.04 with their modifications. Following is thier cfg.mk settings for ethernet.
#
# Supported values: ipu1_0 none
#
FATFS_PROC_TO_USE=none
#
# Supported values: ipu1_0 ipu1_1 none
#
NDK_PROC_TO_USE=ipu1_1
#Used to control TFDTP stack (supported only when NDK_PROC_TO_USE = ipu1_1)
NSP_TFDTP_INCLUDE=yes
Do you see any issues?
Best regards,
Ken