This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TDA2EVM5777: Nothing Display in LCD during Video and Display use case

Part Number: TDA2EVM5777
Other Parts Discussed in Thread: DRA742, PMP

Tool/software: Linux

Hi,

i try to run a example on tda2x board with camera connection and LCD monitor. i prepare the boot SD card as per user manual instructions. i insert the card in to the Board and also connect the LCD monitor. but after the power up the board nothing is display. how i debug the problem nothing is display on the monitor. please help me how to solve the problem

thank you 

  • Hi vijendra,
    Refer section 3.3 of VisionSDK_Linux_UserGuide.pdf to have display over LCD
    3.3 Build Linux Vision SDK for LCD display (M4 Display)
    Note: Only TDA2xx and TDA2ex support 10.1” LG LCD.
     You must follow all the steps in software installation and build.
     Change the dtb picked in the uenv.txt from
    fdtfile=dra7-evm-infoadas.dtb  fdtfile= dra7-evm-infoadas-lcd-lg.dtb for tda2xx
    fdtfile=dra72-evm-infoadas.dtb  fdtfile=dra72-evm-infoadas-lcd-lg.dtb for tda2ex

    Regards
    Surya
  • Hi,

    Have you changed the .dtb file for LCD.
    Please use dra7-evm-infoadas-lcd-lg.dtb file.
    Rename it in uenv.txt file placed in your boot partition .

    Regards,
    Anuj
  • Hi Anuj

    thanks for reply.

    one more thing i want to share that we do not have LG 10' LCD monitor. i have samsung 21' inch LCD display. i connect the TDA2x board with Samsung Display by HDMI port.

    thank you

  • Hello

    Now we can interface the UART console with the Host machine. 

    we use the GTKterm software for interface the console.

    but when we reset the board   through the console it show the error like that 

    reset

    resetting ...

     

    U-Boot SPL 2016.05-00013-g3331a8a6168f (Feb 21 2019 - 13:38:34)

    DRA752-GP ES1.1

    no pinctrl for ddr_1_8v

    ** First descriptor is NOT a primary desc on 1:1 **

    *** Warning - bad CRC, using default environment

     

    Trying to boot from MMC1

    reading dra7-ipu2-fw.lzop

    spl_load_file_fat: error reading file dra7-ipu2-fw.lzop, err - -1

    spl: error reading image dra7-ipu2-fw.lzop, err - -1

    Error loading remotecore IPU2!,Continuing with boot ...

    reading dra7-dsp1-fw.lzop

    spl_load_file_fat: error reading file dra7-dsp1-fw.lzop, err - -1

    spl: error reading image dra7-dsp1-fw.lzop, err - -1

    Error loading remotecore DSP1!,Continuing with boot ...

    reading dra7-dsp2-fw.lzop

    spl_load_file_fat: error reading file dra7-dsp2-fw.lzop, err - -1

    spl: error reading image dra7-dsp2-fw.lzop, err - -1

    Error loading remotecore DSP2!,Continuing with boot ...

    reading dra7-ipu1-fw.lzop

    spl_load_file_fat: error reading file dra7-ipu1-fw.lzop, err - -1

    spl: error reading image dra7-ipu1-fw.lzop, err - -1

    Error loading remotecore IPU1!,Continuing with boot ...

    *** Warning - bad CRC, using default environment

     

    reading u-boot.img

    reading u-boot.img

    reading u-boot.img

    reading u-boot.img

     

     

    U-Boot 2016.05-00013-g3331a8a6168f (Feb 21 2019 - 13:38:34 +0530)

     

    CPU  : DRA752-GP ES1.1

    Model: TI DRA742

    Board: DRA74x EVM REV G.0

    DRAM:  1.5 GiB

    MMC:   mmc@4809c000: fail to find hs-rev11 mode FDT_ERR_NOTFOUND

    mmc@4809c000: fail to find sdr25-rev11 mode FDT_ERR_NOTFOUND

    mmc@4809c000: fail to find sdr12-rev11 mode FDT_ERR_NOTFOUND

    mmc@480b4000: fail to find hs-rev11 mode FDT_ERR_NOTFOUND

    OMAP SD/MMC: 0, OMAP SD/MMC: 1

    ** First descriptor is NOT a primary desc on 1:1 **

    *** Warning - bad CRC, using default environment

     

    GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645

    part_get_info_efi: *** ERROR: Invalid GPT ***

    GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645

    part_get_info_efi: *** ERROR: Invalid Backup GPT ***

    ERROR: cannot find partition: 'userdata'

     

    at arch/arm/cpu/armv7/omap-common/utils.c:199/mmc_get_part_size()

    Warning: fastboot.userdata_size: unable to calc

    SCSI:  SATA link 0 timeout.

    AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode

    flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst 

    scanning bus for devices...

    Found 0 device(s).

    Net:   

    Warning: ethernet@48484000 using MAC address from ROM

    eth0: ethernet@48484000

    Hit any key to stop autoboot:  0 

    ## Error: "board_findfdt" not defined

    switch to partitions #0, OK

    mmc0 is current device

    SD/MMC found on device 0

    reading boot.scr

    ** Unable to read file boot.scr **

    reading uEnv.txt

    173 bytes read in 3 ms (55.7 KiB/s)

    Loaded env from uEnv.txt

    Importing environment from mmc0 ...

    switch to partitions #0, OK

    mmc0 is current device

    SD/MMC found on device 0

    ** File not found /boot/zImage **

    ** First descriptor is NOT a primary desc on 1:1 **

    switch to partitions #0, OK

    mmc1(part 0) is current device

    ** First descriptor is NOT a primary desc on 1:1 **

    mmc - MMC sub system

     

    Usage:

    mmc info - display info of the current MMC device

    mmc read addr blk# cnt

    mmc write addr blk# cnt

    mmc erase blk# cnt

    mmc rescan

    mmc part - lists available partition on current mmc device

    mmc dev [dev] [part] - show or set current mmc device [partition]

    mmc list - lists available devices

    mmc hwpartition [args...] - does hardware partitioning

      arguments (sizes in 512-byte blocks):

        [user [enh start cnt] [wrrel {on|off}]] - sets user data area attributes

        [gp1|gp2|gp3|gp4 cnt [enh] [wrrel {on|off}]] - general purpose partition

        [check|set|complete] - mode, complete set partitioning completed

      WARNING: Partitioning is a write-once setting once it is set to complete.

      Power cycling is required to initialize partitions after set to complete.

    mmc bootbus dev boot_bus_width reset_boot_bus_width boot_mode

     - Set the BOOT_BUS_WIDTH field of the specified device

    mmc bootpart-resize <dev> <boot part size MB> <RPMB part size MB>

     - Change sizes of boot and RPMB partitions of specified device

    mmc partconf dev boot_ack boot_partition partition_access

     - Change the bits of the PARTITION_CONFIG field of the specified device

    mmc rst-function dev value

     - Change the RST_n_FUNCTION field of the specified device

       WARNING: This is a write-once field and 0 / 1 / 2 are the only valid values.

    mmc setdsr <value> - set DSR register value

     

    mmc - MMC sub system

     

    Usage:

    mmc info - display info of the current MMC device

    mmc read addr blk# cnt

    mmc write addr blk# cnt

    mmc erase blk# cnt

    mmc rescan

    mmc part - lists available partition on current mmc device

    mmc dev [dev] [part] - show or set current mmc device [partition]

    mmc list - lists available devices

    mmc hwpartition [args...] - does hardware partitioning

      arguments (sizes in 512-byte blocks):

        [user [enh start cnt] [wrrel {on|off}]] - sets user data area attributes

        [gp1|gp2|gp3|gp4 cnt [enh] [wrrel {on|off}]] - general purpose partition

        [check|set|complete] - mode, complete set partitioning completed

      WARNING: Partitioning is a write-once setting once it is set to complete.

      Power cycling is required to initialize partitions after set to complete.

    mmc bootbus dev boot_bus_width reset_boot_bus_width boot_mode

     - Set the BOOT_BUS_WIDTH field of the specified device

    mmc bootpart-resize <dev> <boot part size MB> <RPMB part size MB>

     - Change sizes of boot and RPMB partitions of specified device

    mmc partconf dev boot_ack boot_partition partition_access

     - Change the bits of the PARTITION_CONFIG field of the specified device

    mmc rst-function dev value

     - Change the RST_n_FUNCTION field of the specified device

       WARNING: This is a write-once field and 0 / 1 / 2 are the only valid values.

    mmc setdsr <value> - set DSR register value

     

    Booting from eMMC ...

    Wrong Image Format for bootm command

    ERROR: can't get kernel image!

    => 

    thank you 

    vijender

  • Hi Vijendra,
    If you are connecting any display device through HDMI, no need to change anything in uenv.txt file
    Default display device selected is display over HDMI

    Boot issue:
    Could you please check boot mode PINs are set to SD boot ?

    Regards
    Surya