Hi,
I have been looking at the DM365 chip and I am interested in the SPI Boot Mode, Once we set BTSEL[2:0] to 101 the RBL will automatically try to copy a UBL to the internal memory of the ARM. We want to connect a SPI Flash to the SPI0 interface of the DM365.
1.) Where does the RBL begin to look for the UBL (in page 0)?
2.) How does one initially place the UBL into the SPI Flash?
3.) From what I see, it seems that the UBL will be customized, to begin loading the Linux Montavista from the SPI Flash as well, is there a document or procedure on how to get started in developing a proper uboot forthe DM365?
Thanks in advance.