Part Number: TDA2PXEVM
Tool/software: TI-RTOS
Hi All,
I am working on VSDK 3.05. I am working on a decoder which takes data from 4 cameras and sends the data on the 2 lanes of CSI2 PHY2 with the resolution 640x480.
As the decoder contains an ISP I am not using M2mIspLink and Alg_IssAewb. The use case contains Capture + Display. I am having issues in setting display params.
I am refering to the use case iss_capture_isp_simcop_display.
My doubt is in the function UseCase_SetAppPrms().As M2mIsp link is not used I have not used the following variables in my use case object.
IssM2mSimcopLink_ConfigParams simcopConfig;
vpsissldcConfig_t ldcCfg;
vpsissvtnfConfig_t vtnfCfg;
IssM2mSimcopLink_OperatingMode simcopMode;
Bool bypassVtnf;
Bool bypassLdc;
Due to this I have not set simcopMode, bypassVtnf,, bypassLdc in function UseCase_SetAppPrms() .
Will this create any issues, as I do not have the decoder with me right now,I cannot test it.So just wanted to ask whether this is fine or not?
Regards,
Deepika