This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2: To add the 5th AWR1243 here are the pinout changes

Part Number: TDA2
Other Parts Discussed in Thread: AWR1243

To add the 5th AWR1243 here are the pinout changes we are planning to the cascade radar reference design. Can you confirm we are not using any pins incorrectly?

 

With Muxmode = 7

Pins needed for 5th AWR1243:

Pin          remove                                                                                add

C14      open                                                                                 vin6a_fld0                          

G12        I2C5_SDA                                                                           vin6a_vsyn 

F12        I2C5_SCL                                                                              vin6a_hsyn

B13         TDA_FPGA_SPI_SEL_A_GPIO5_12                             VIN6A_D13

A12        TDA_FPGA_SPI_SEL_B_GPIO4_17                             VIN6A_D12                                

E14         TDA_AWR1_GPIO0_GPIO4_18                                   VIN6A_D11

A13        TDA_AWR1_GPIO1_GPIO6_4                                     VIN6A_D10

G14        TDA_AWR1_GPIO2_GPIO6_5                                     VIN6A_D9

F14       open                                                                                      VIN6A_D8

B12        TDA_AWR2_SPI_INT_GPIO5_10                                VIN6A_D15

A11        TDA_AWR3_SPI_INT_GPIO5_11                                VIN6A_D14

D14        open                                                                                     VIN6A_DE0

A19        open                                                                                     VIN6A_D7

C15         open                                                                                     VIN6A_D5

A16        open                                                                                     VIN6A_D4

A18        open                                                                                     VIN6A_D6

B18         open                                                                                     VIN6A_D3

B19        open                                                                                     VIN6A_D1

C17        open                                                                                     VIN6A_D0

F15         open                                                                                     VIN6A_D2

E17         open                                                                                     VIN6A_CLK0

D18        open                                                                                     VIN6A_D0

 

Move these signals to new pins:

Pin          remove                                                                                add

AA3        TDA_VIN4A_D20                                                              I2C5_SDA               

AB9        TDA_VIN4A_D21                                                              I2C5_SCL

C18         TDA_VIN4A_D16                                                              TDA_AWR2_SPI_INT_GPIO5_10

A21        TDA_VIN4A_D17                                                              TDA_AWR3_SPI_INT_GPIO5_11

G16        TDA_VIN4A_D18                                                              TDA_AWR1_GPIO0_GPIO4_18

D17        TDA_VIN4A_D19                                                              TDA_AWR1_GPIO1_GPIO6_4

AB3        TDA_VIN4A_D22                                                              TDA_AWR1_GPIO2_GPIO6_5

R6           TDA_VIN3A_MUX_D16                                                 TDA_FPGA_SPI_SEL_A_GPIO5_12

T9           TDA_VIN3A_MUX_D17                                                 TDA_FPGA_SPI_SEL_B_GPIO4_17

 

  • Hi Zach,

    Please find some feedback on the pin list below:

    C18 TDA_VIN4A_D16 TDA_AWR2_SPI_INT_GPIO5_10 --> Pad does not support GPIO.
    A21 TDA_VIN4A_D17 TDA_AWR3_SPI_INT_GPIO5_11 --> Pad does not support GPIO
    G16 TDA_VIN4A_D18 TDA_AWR1_GPIO0_GPIO4_18 --> Pad does not support GPIO
    D17 TDA_VIN4A_D19 TDA_AWR1_GPIO1_GPIO6_4 --> Pad does not support GPIO
    AB3 TDA_VIN4A_D22 TDA_AWR1_GPIO2_GPIO6_5 --> Pad does not support GPIO
    R6 TDA_VIN3A_MUX_D16 gpio7_3
    T9 TDA_VIN3A_MUX_D17 gpio7_4

    Others are okay.

    Thanks and Regards,
    Piyali