Team,
-Are you aware of any IEEE 1588v2 implementation running on the C66x (via the NDK stack) and using the GMAC_SW (not the PRU-ICSS) ?
Are there any Third party offering it?
Is it a use case that we directly support?
-We do provide the pre-build NDK 3.40 in RTOS SDK 5.02.
As it been validated as well for the C66x?
Is there a way to access the NDK 3.40 docs directly without to have to install the complete RTOS SDK?
I can only find high level NDK docs on the SDK page:
http://software-dl.ti.com/processor-sdk-rtos/esd/docs/05_02_00_10/rtos/index_Foundational_Components.html#ndkBut not the details like it use to be provided. For example for NDK 2.25 we know exactly what was tested:
http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/ndk/2_25_01_11/exports/ndk_2_25_01_11/ndk_2_25_01_11_release_notes.html#Validation
Thanks in advance,
A.