Part Number: AM3358
Tool/software: Linux
We have a custom board. we can power 2 ways like in beaglebone black .via USB and direct DC voltage.
Now the issue is from uboot when I probe i2c dev 1
when the board is connected on USB power I can communicate to the I2C dev on bus 1 but when I connect the board on DC power then I am unable to connect to I2C dev 1 . The I2C slave is not detected when on DC power and it gets detected when on USB.
Same is the case with Linux
Thanks,