Tool/software: Linux
Hi,
I created a bootable SD card using the create-sd-card.sh script that ships with the TI SDK 05.00.00.02. I'm able to boot from the SD card through the usual method of holding the S1 button.
I also have a working image at the eMMC that I'd like to keep. I don't want to erase it or to flash the SD card contents into the eMMC.
So, how could I boot from the SD card without pressing the S1 button? Currently, I don't have any uEnv.txt file in the boot partition of the SD card.
Regards,
Bruno.