Other Parts Discussed in Thread: TDA2
Tool/software: Linux
Hi,
I manage to enable GST encode/decode based on IPUMM for VSDK 3.05. According to <<Vision SDK Linux User Guide>>, there are two options to enable IPUMM.
1. IPUMM on VSDK-Linux and IPU-1 as primary IPU for Vision-SDK
Per the instructions in the guide, It works fine for me.
2. IPUMM and VSDK-Linux on IPU-2
But for the option 2, I still cannot figure it out. I follow section 2.4.2.2 to prepare ipumm, Codec Engine and Framework components. IVAHD is set to no in the corresponding cfg.mk. Whether or not to enbable IPUMM in the same file, I always encounter assert failure with the resultant apps.out launch. Please help if something is missing. Thanks!
Regards,
Simon
[HOST] [HOST ] 3151.468401 s: SELECT_1 : Init done - linkid-0x0
[HOST] [HOST ] 3151.468492 s: GATE_0 : Init done - linkid-0x0
[HOST] [HOST ] 3151.468614 s: GATE_1 : Init done - linkid-0x0
[HOST] [HOST ] 3151.468706 s: GATE_2 : Init done - linkid-0x0
[HOST] [HOST ] 3151.468797 s: GATE_3 : Init done - linkid-0x0
[HOST] [HOST ] 3151.468889 s: SGXFRMCPY_0 : Init done - linkid-0x2000046
[HOST] [HOST ] 3151.468980 s: ZMCAMERA_0 : Init done - linkid-0x2000066
[HOST] [HOST ] 3151.469072 s: ZMOutput_0 : Init done - linkid-0x2000067
[HOST] [HOST ] 3151.469102 s: SYSTEM: Initializing A15 Links ... DONE !!!
[HOST] [HOST ] 3151.469163 s: SYSTEM: IPC: [IPU1-0] Notify send failed (Socket operation on non-socket, 88) !!!
[HOST] [HOST ] 3151.469163 s: SYSTEM: MSGQ: [IPU1-0] MsgQ send failed !!!
[HOST] [HOST ] 3151.469163 s: SYSTEM: System A15 Init Done !!!
[HOST] [HOST ] 3151.469316 s: SYSTEM: IPC: [IPU1-0] Notify send failed (Socket operation on non-socket, 88) !!!
[HOST] [HOST ] 3151.469316 s: SYSTEM: MSGQ: [IPU1-0] MsgQ send failed !!!
[HOST] [HOST ] 3151.469316 s: NETWORK_CTRL: Starting Server (port=5000) !!!
[HOST] [HOST ] 3151.469377 s: NETWORK_CTRL: Starting Server ... DONE (port=5000) !!!
ASSERT (chains_common.c|ChainsCommon_appCtrlCommonInit|296)