Other Parts Discussed in Thread: TMS320DM365, TPA2001D1
Hello all
I am new to TI DM365, and TI processors in general. I discover audio too!
I was comparing the DM355 and DM365 for a low cost system including sound capture. It has not to be CD perfect sound so a voice codec can match my requirements. On the DM355 there is no voice codec, and all schematics I saw used the TLV series devices I2S connected to the DM355, on which a MIC and a loud speaker were connected.
On the other hand, on DM365 I saw application schematics connecting directly the MIC and the loud Speaker to the voice codec.
My question is : is the DaVinci DM365 powerful enough to power a loud speaker of let's say between 0.5W to 1W power ?
Thanks for your reply.