This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TDA2: [Vlib in vision sdk]. Is Vlib function thread safe ?

Part Number: TDA2

Tool/software: TI-RTOS

Hi Ti,

I am currently use Vlib with links-chain concept in the latest rtos vision SDK for TI TDA2X (2 dsp core).

I have used vlib's connected component function and it works fine.

Now i plane to use this function to multiple 'link'(thread) on 2 dsp cores.

(2 links on 2 dsp core each. total 4 links)

Problem is, this function does not work correctly when I use it with multiple link with 2 dsp cores. 

(It works fine if I use just one link on one dsp core.)

All the memories for each connected component functions are allocated in inside of link, and, I checked that the memories not invaded each other.

They have a different address.

But It seems that the results of each functions are mixed.

Have Vlib function tested with multiple link? Is it thread safe ?