Part Number: TDA2
Tool/software: Linux
Our current problem: When the DVR function is always turned on, if we want to add other functions, the efficiency of the DDR bus will become lower, resulting in other CPU performance degradation, and the performance of the TDA2Sx chip cannot be fully utilized.
Question 1: At present, our hardware design TDA2 DDR bandwidth is more than 8,000 MB, but why the DDR bandwidth of the emif1 plus emif2 port shown in the figure below is more than 4,000 MB? What are its main influence factors? (We didn't use ECC DDR)
My question 2: How can we optimize the IVA module? The frequency of accessing the DDR by the IVA module is reduced to about 500 MB/s. As shown in the red box below, the IVA access DDR frequency takes up 55% of the total DDR bandwidth.
At present, the DVR solution we use is Capture to capture 4 channels of 1280x720P@30 frames, splicing 4 original images into 1 channel 2560*1440 image, then inputting to the encode module to generate H264 code stream, and finally encapsulating H264 code stream as Mp4 file.