Tool/software: TI-RTOS
IDKAM437x
Hello, I am modifying ethercat_slave_demo project, adding more tasks,
I simply added a server code(TCP_echo_Server) that runs on CPSW ethernet, my main.c is below:
int main(){
TaskP_Params taskParams;
Board_init(BOARD_INIT_PINMUX_CONFIG | BOARD_INIT_MODULE_CLOCK |
BOARD_INIT_ICSS_PINMUX | BOARD_INIT_UART_STDIO);
TaskP_Params_init(&taskParams);
taskParams.priority = 4;
taskParams.stacksize = 2048*TIESC_TASK_STACK_SIZE_MUL;
ecat_hndl = TaskP_create(ethercat_slave_task, &taskParams);
/* Chip configuration MII/RMII selection */
CpswPortMacModeSelect(1, ETHERNET_MAC_TYPE_RGMII);
CpswPortMacModeSelect(2, ETHERNET_MAC_TYPE_RGMII);
TaskP_Params_init(&taskParams);
taskParams.priority = 2;
taskParams.stacksize = 0x2000;
tcp_hndl = TaskP_create(TCP_echo_Server, &taskParams);
NIMUDeviceTable[nimu_device_index++].init = &CpswEmacInit ; //nimu_device_index = 0
NIMUDeviceTable[nimu_device_index].init = NULL ;
OSAL_OS_start();
}
Thanks in advance.