This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/PROCESSOR-SDK-AM437X: Ethercat Port0 & Port1 connection issue

Part Number: PROCESSOR-SDK-AM437X

Tool/software: TI-RTOS

Hi Champs:

#1. We tested this prebuild FW on AM437 IDK: pru_icss_ethercat_slave_prebuilt_01.00.07.02

#2. Using TwinCat 3.1 for testing the Ethercat Port 0 / 1.

      Here is the issue we found:

               Case 1:

                  Testing with TwinCat by using Port 0 is okay.

                  Then, switch the Ethernet Cable to Port 1, the Twincat cannot work with Port 1.

             Case 2:                  

                  Testing with TwinCat by using Port 1 is okay.

                  Then, switch the Ethernet Cable to Port 0,  the Twincat works.

                  Then, switch back to the  Port 1, the Twincat will not work.

       Please comment on this if this is a real issue or not, if yes, how to solve?

BR Rio