This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4376: Power-up Sequencing

Part Number: AM4376

Hi

By using simplified power sequence (Datasheet Figure 5-8  *) can I connect VDDS_DDR and VDD_MPU together? Because they have voltages near each other. 1.35V for DDR3L that can work with 1.325V (for VDD_MPU), so if I connect them there would be one less DC/DC. Power sequence would be as follow: 3.3V --> 1.8V --> 1.325V (VDDS_DDR, VDD_MPU) --> 1.1V (VDD_CORE, CAP_VDD_RTC)

I this a valid configuration?

 

* Simplified Power Sequencing With RTC Feature Disabled, Dual-Voltage IOs Configured as 3.3 V

 

Regards,

Robert