Other Parts Discussed in Thread: TMS320DM355
There are several of us over in the gstreamer forum (at https://gstreamer.ti.com/ ) that are having the same problem and no luck finding help, so I thought I would try this forum.
I have compiled gstreamer from the source of gst-ti-plugin-full-0.99.00. I can successfully play back the standard davincieffect.mpeg4 elementary file using ./decode_elementary.sh. But when I try to play back a .avi file I get:
./decode_avi.sh -f videos/testFull.avi
gst-inspect TIViddec2
gst-inspect mad
gst-inspect osssink
*********** Pipeline Settings *************
platform = dm355
audio_plugin = mad
audio_plugin_args =
soundStd = oss
video_plugin = TIViddec2
video_plugin_args =
dispStd = fbdev
dispDevice = /dev/fb/3
videoStd = D1_NTSC
videoOutput = COMPOSITE
resizer = FALSE
accelFrameCopy = TRUE
gst-launch --gst-debug-no-color --gst-debug=TI*:2 filesrc location=videos/testFull.avi ! typefind ! avidemux name=demux demux.audio_00 ! queue max-size-buffers=
1200 max-size-time=0 max-size-bytes=0 ! typefind ! mad ! audioconvert ! osssink demux.video_00 ! typefind ! TIViddec2 ! TIDmaiVideoSink displayStd=fbdev display
Device=/dev/fb/3 videoStd=D1_NTSC videoOutput=COMPOSITE resizer=FALSE accelFrameCopy=TRUE
Setting pipeline to PAUSED ...
Pipeline is PREROLLING ...
ERROR: from element /GstPipeline:pipeline0/GstAviDemux:demux: Internal data stream error.
Additional debug info:
gstavidemux.c(4115): gst_avi_demux_loop (): /GstPipeline:pipeline0/GstAviDemux:demux:
streaming stopped, reason not-negotiated
ERROR: pipeline doesn't want to preroll.
Setting pipeline to NULL ...
FREEING pipeline ...
Note that my testFull.avi file has played back successfully using a precompiled version of gstreamer and all of the same settings. I get no errors when compiling gstreamer. I need to modify gsttidmaivideosink.c, so I can't just use the canned version of gstreamer. I get the same error with gst-ti-plugin-full-1.00.02.
Any ideas on where I should look?
I am using dvsdk_1_30_00_40, dmai_1_16_00_03, xdc_3_00_04, and RHEL4.
Thanks
-Vim