Part Number: BEAGLEBK
Tool/software: TI-RTOS
Hi,
Here is the system setup that I am using:
Platform: Beaglebone Black
EDMA3 Low Level Driver 2.12.5
NDK 3.40.1.01
SYS/BIOS 6.73.1.01
am335x PDK 1.0.13
Base Source: NIMU_BasicExample_bbbAM335x_armExampleProject
I want to use Sockets API to send/receive data on my host computer. First I tried with making my board as client and host computer as server. The code of the client looks as follows. I start the server at my host computer and start debugging the application. The application exits with Data Abort exception when I try to connect to the host computer.
void client()
{
SOCKET s;
int status;
char data[] = "Hello";
struct sockaddr_in cli_addr;
s = socket(AF_INET, SOCK_DGRAM, IPPROTO_UDP);
if (s <0)
{
UART_printf("Socket not created: %d\n", fdError());
}
memset(&cli_addr, 0, sizeof(cli_addr));
cli_addr.sin_family = AF_INET;
cli_addr.sin_addr.s_addr = inet_addr("192.168.1.10");
cli_addr.sin_port = 17225;
int err = NDK_connect(s, (struct sockaddr *)&cli_addr, sizeof(cli_addr));
if(err<0)
{
UART_printf("%x\n",fdError());
}
while(1)
{
err = NDK_send(s, data, sizeof(data), 0);
if(err<0)
{
UART_printf("%x\n",fdError());
}
}
}
Then, I try to make my board as server and host computer as client. The code for the server app on board looks as follows. I launch the application on board and connect the host computer using telnet. The host computer connects successfully. However, I am not able to receive any data on the board (NDK_recvfrom)and I get the fdError as 16 (DEVICE_BUSY in serrno.h). I am not able to understand this strange behavior.
SOCKET s;
struct sockaddr_in local_addr, cli_addr;
char buffer[256];
s = NDK_socket(AF_INET, SOCK_STREAM, 0);
if (s == INVALID_SOCKET)
{
UART_printf("%x\n", fdError());
}
/*I am adding a comment 3*/
memset(&local_addr,0,sizeof(local_addr));
local_addr.sin_family = AF_INET;
local_addr.sin_addr.s_addr = INADDR_ANY;
local_addr.sin_port = 17225;
int err = NDK_bind(s,(struct sockaddr *)&local_addr, sizeof(local_addr));
if(err<0)
{
UART_printf("%d\n", fdError());
}
int size = sizeof(cli_addr);
err = NDK_listen(s, 10);
UART_printf("%d\n", err);
if(err<0)
{
UART_printf("%d\n", fdError());
}
SOCKET computer = NDK_accept(s,(struct sockaddr *)&cli_addr, &size);
if(computer ==INVALID_SOCKET)
{
UART_printf("Error: %x\n", fdError());
}
while(1)
{
int bytes = NDK_recvfrom(s, buffer,sizeof(buffer),0,(struct sockaddr *)&cli_addr, &size);
if(bytes<0)
{
UART_printf("Error: %x\n", fdError());
}
if (bytes>0)
{
int bytesSent = sendto(s, buffer, bytes, 0,
(struct sockaddr *)&cli_addr, sizeof(cli_addr));
}
}
I would request TI to please help me with following:
1. Is there any TCP/UDP Echo example for AM335x or Beaglebone Black? (I know there are examples from TIVA C and I followed the same procedure, what is in there but I get exceptions)
2. It seems to me that something is wrong with the configuration of the Ethernet. Do you think above errors are because of incorrect configuration?
Regards
Vishav