Part Number: AM3352
Hi Sitara support Team,
I would like to confirm about the maximum value (10 or 5 ns) of the following signal transition time.
- DCAN Timing Conditions
- DMTimer Timing Conditions
- JTAG Timing Conditions
- LCD Controller Timing Conditions
- UART Timing Conditions
- UART (PRU-ICSS)Timing Conditions
Q1. What is the background to add the specified max values ??in the latest datasheet?
Q2. Will it cause a malfunction even with a monotonically increasing signal of 1 ms?
Q 3. If it must be complied with the specified max values,
can you suggest the countermeasure plan?
Q4. Is the max value same in 3.3V and 1.8V supply?
I need to explain them to my customer who thinks that the max values are unreasonable
to guarantee the design with ordinary logic ICs.
Best regards,
Kanae