Tool/software: TI-RTOS
Hello.
I'm using ethernetip_adapter project and it could communicate by TCP/IP Ethernet well.
I would like to confirm TCP/IP Ethernet communication between master device and several AMIC110 slave devices connected with daisy chain as below.
If master communicate with slave B only, which Is the communication pass of case 1 and case 2?
If it is case 2, can I set to run as case 1 only and could you tell me how to configure?
Regards,
U-SK