This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3357: Which processors supports a MPU frequency of 800MHz and a DDR3 frequency of 400MHz?

Part Number: AM3357


Hi,

I use the AM3357. So far with an MPU frequency of 720MHz and a DDR3 frequency of 303MHz. Now i want to increase the frequency of the MPU to 800MHz and the DDR3 frequency to 400MHz. How can i distinguish in the firmware which processors (AM3357, XAM3357) support the higher frequencies? Is there a way to distinguish XAM3357 and AM3357 processors in the firmware?

Thanks and Regards

Martin