Part Number: AM5728
Other Parts Discussed in Thread: TLVH431, TMDXIDK5718, SN74LVC2G241, TPS659037, AM5718, TPS3808
We have designed a custom board around the AM5728 and we have experienced 3 failures (out of a total of 15 assemblies). None of the failures are consistent but they all seem to have something to do with the power rails on the AM5728. The first failure was fixed by replacing the CPU, the other two boards are out for rework and we should be receiving them back shortly.
- The first CPU failure had a low resistance between VCC_CORE and VDD_1V8
- another had 5 ohms to ground on the core voltage
- a third had a combination of lower than expected resistances from one core voltage to several others and failure to boot
There are two other boards that are experiencing unexplained behavior that seems to be related to the CPU not behaving normally (an interface stopped working - SDIO & eMMC0).
I've looked over a lot of TI documentation including the schematic checklist and hardware design guide but haven't found anything that looks like a problem in our design.
Lastly the three boards all have worked well for weeks before they stopped functioning - then suddenly on a power cycle they refused to boot.
My question is - can we have the CPU's sent to TI for failure analysis? This will give us a hint as to the cause of the problem(s) so we can be confident in the design of the board before we go to production.
Thanks in advance!