This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEVM6678: Read data from external device to the DSP via SPI protocol

Part Number: TMDSEVM6678

Hi,

I want to read the data that is stored in an external FPGA board (De0 nano altera FPGA) to the DSP board for signal processing via SPI master. Now, I am unable to find any proper documentation regarding the SPI functions and how do they work or any example project. I found these two files (attached below) which I think would help in my case.

/******************************************************************************
 * Copyright (c) 2011 Texas Instruments Incorporated - http://www.ti.com
 * 
 *  Redistribution and use in source and binary forms, with or without 
 *  modification, are permitted provided that the following conditions 
 *  are met:
 *
 *    Redistributions of source code must retain the above copyright 
 *    notice, this list of conditions and the following disclaimer.
 *
 *    Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the 
 *    documentation and/or other materials provided with the   
 *    distribution.
 *
 *    Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
 *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
 *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
 *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
 *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
 *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
 *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
 *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
 *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
 *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
 *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 * 
 *****************************************************************************/

/******************************************************************************
 *
 * File Name:   evmc66x_spi.c
 *
 * Description: This file implements SPI driver for the NOR flash
 *  
 *****************************************************************************/
 
/************************
 * Include Files
 ************************/
#include "platform_internal.h"


static uint32_t data1_reg_val;

static void 
spi_delay
( 
    uint32_t delay 
)
{
    volatile uint32_t i;

    for ( i = 0 ; i < delay ; i++ ){ };
}


/******************************************************************************
 * 
 * Function:    spi_claim  
 *
 * Description: This function claims the SPI bus in the SPI controller 
 *
 * Parameters:  Uint32 cs       - Chip Select number for the slave SPI device
 *              Uint32 freq     - SPI clock frequency  
 *
 * Return Value: error status
 * 
 ******************************************************************************/
SPI_STATUS 
spi_claim
(
    uint32_t      cs,
    uint32_t      freq
)
{
    uint32_t scalar;

    PLIBSPILOCK()

    /* Enable the SPI hardware */
    SPI_SPIGCR0 = CSL_SPI_SPIGCR0_RESET_IN_RESET;
    spi_delay (2000);
    SPI_SPIGCR0 = CSL_SPI_SPIGCR0_RESET_OUT_OF_RESET;

    /* Set master mode, powered up and not activated */
    SPI_SPIGCR1 =   (CSL_SPI_SPIGCR1_MASTER_MASTER << CSL_SPI_SPIGCR1_MASTER_SHIFT)   |
                    (CSL_SPI_SPIGCR1_CLKMOD_INTERNAL << CSL_SPI_SPIGCR1_CLKMOD_SHIFT);
    
    
    /* CS0, CS1, CLK, Slave in and Slave out are functional pins */
    if (cs == 0) {
        SPI_SPIPC0 =    (CSL_SPI_SPIPC0_SCS0FUN0_SPI << CSL_SPI_SPIPC0_SCS0FUN0_SHIFT) |
                        (CSL_SPI_SPIPC0_CLKFUN_SPI << CSL_SPI_SPIPC0_CLKFUN_SHIFT)     |
                        (CSL_SPI_SPIPC0_SIMOFUN_SPI << CSL_SPI_SPIPC0_SIMOFUN_SHIFT)   |
                        (CSL_SPI_SPIPC0_SOMIFUN_SPI << CSL_SPI_SPIPC0_SOMIFUN_SHIFT);
    } else if (cs == 1) {
        SPI_SPIPC0 =    ((CSL_SPI_SPIPC0_SCS0FUN1_SPI << CSL_SPI_SPIPC0_SCS0FUN1_SHIFT) |
                        (CSL_SPI_SPIPC0_CLKFUN_SPI << CSL_SPI_SPIPC0_CLKFUN_SHIFT)     |
                        (CSL_SPI_SPIPC0_SIMOFUN_SPI << CSL_SPI_SPIPC0_SIMOFUN_SHIFT)   |
                        (CSL_SPI_SPIPC0_SOMIFUN_SPI << CSL_SPI_SPIPC0_SOMIFUN_SHIFT)) & 0xFFFF;
    }
    
    /* setup format */
    scalar = ((SPI_MODULE_CLK / freq) - 1 ) & 0xFF;

    if ( cs == 0) {
        SPI_SPIFMT0 =   (8 << CSL_SPI_SPIFMT_CHARLEN_SHIFT)               |
                        (scalar << CSL_SPI_SPIFMT_PRESCALE_SHIFT)                      |
                        (CSL_SPI_SPIFMT_PHASE_DELAY << CSL_SPI_SPIFMT_PHASE_SHIFT)     |
                        (CSL_SPI_SPIFMT_POLARITY_LOW << CSL_SPI_SPIFMT_POLARITY_SHIFT) |
                        (CSL_SPI_SPIFMT_SHIFTDIR_MSB << CSL_SPI_SPIFMT_SHIFTDIR_SHIFT);
    }else if ( cs == 1) {
        SPI_SPIFMT0 =   (16 << CSL_SPI_SPIFMT_CHARLEN_SHIFT)               |
                        (scalar << CSL_SPI_SPIFMT_PRESCALE_SHIFT)                      |
                        (CSL_SPI_SPIFMT_PHASE_NO_DELAY << CSL_SPI_SPIFMT_PHASE_SHIFT)     |
                        (CSL_SPI_SPIFMT_POLARITY_LOW << CSL_SPI_SPIFMT_POLARITY_SHIFT) |
                        (CSL_SPI_SPIFMT_SHIFTDIR_MSB << CSL_SPI_SPIFMT_SHIFTDIR_SHIFT);
    }
    
    /* hold cs active at end of transfer until explicitly de-asserted */
    data1_reg_val = (CSL_SPI_SPIDAT1_CSHOLD_ENABLE << CSL_SPI_SPIDAT1_CSHOLD_SHIFT) |
                    (0x02 << CSL_SPI_SPIDAT1_CSNR_SHIFT);
     if (cs == 0) {
         SPI_SPIDAT1 =   (CSL_SPI_SPIDAT1_CSHOLD_ENABLE << CSL_SPI_SPIDAT1_CSHOLD_SHIFT) |
                         (0x02 << CSL_SPI_SPIDAT1_CSNR_SHIFT);
     } 

    /* including a minor delay. No science here. Should be good even with
    * no delay
    */
    if (cs == 0) {
        SPI_SPIDELAY =  (8 << CSL_SPI_SPIDELAY_C2TDELAY_SHIFT) |
                        (8 << CSL_SPI_SPIDELAY_T2CDELAY_SHIFT);
        /* default chip select register */
        SPI_SPIDEF  = CSL_SPI_SPIDEF_RESETVAL;        
    } else if (cs == 1) {    
        SPI_SPIDELAY =  (6 << CSL_SPI_SPIDELAY_C2TDELAY_SHIFT) |
                        (3 << CSL_SPI_SPIDELAY_T2CDELAY_SHIFT);
    }
    
    /* no interrupts */
    SPI_SPIINT0 = CSL_SPI_SPIINT0_RESETVAL;
    SPI_SPILVL  = CSL_SPI_SPILVL_RESETVAL;

    /* enable SPI */
    SPI_SPIGCR1 |= ( CSL_SPI_SPIGCR1_ENABLE_ENABLE << CSL_SPI_SPIGCR1_ENABLE_SHIFT );

    if (cs == 1) {
        SPI_SPIDAT0 = 1 << 15; 
        spi_delay (10000);        
        /* Read SPIFLG, wait untill the RX full interrupt */
        if ( (SPI_SPIFLG & (CSL_SPI_SPIFLG_RXINTFLG_FULL<<CSL_SPI_SPIFLG_RXINTFLG_SHIFT)) ) {                
            /* Read one byte data */
            scalar = SPI_SPIBUF & 0xFF;
            /* Clear the Data */
            SPI_SPIBUF = 0;
        }
        else {
            /* Read one byte data */
            scalar = SPI_SPIBUF & 0xFF;
            return SPI_EFAIL;
        }
    }
    return SPI_EOK;
}

/******************************************************************************
 * 
 * Function:    spi_release  
 *
 * Description: This function releases the bus in SPI controller 
 *
 * Parameters:  None
 *
 * Return Value: None
 * 
 ******************************************************************************/
void 
spi_release
(
    void
)
{
    /* Disable the SPI hardware */
    SPI_SPIGCR1 = CSL_SPI_SPIGCR1_RESETVAL;

    PLIBSPIRELEASE()
}

/******************************************************************************
 * 
 * Function:    spi_xfer  
 *
 * Description: This function sends and receives 8-bit data serially
 *
 * Parameters:  uint32_t nbytes   - Number of bytes of the TX data
 *              uint8_t* data_out - Pointer to the TX data
 *              uint8_t* data_in  - Pointer to the RX data
 *              Bool terminate  - TRUE: terminate the transfer, release the CS
 *                                FALSE: hold the CS
 *
 * Return Value: error status
 * 
 ******************************************************************************/
SPI_STATUS 
spi_xfer
(
    uint32_t              nbytes,
    uint8_t*              data_out,
    uint8_t*              data_in,
    Bool                terminate
)
{
    uint32_t          i, buf_reg;
    uint8_t*          tx_ptr = data_out;
    uint8_t*          rx_ptr = data_in;
    
    
    /* Clear out any pending read data */
    SPI_SPIBUF;
    
    for (i = 0; i < nbytes; i++) 
    {
        /* Wait untill TX buffer is not full */
        while( SPI_SPIBUF & CSL_SPI_SPIBUF_TXFULL_MASK );
        
        /* Set the TX data to SPIDAT1 */
        data1_reg_val &= ~0xFFFF;
        if(tx_ptr) 
        {
            data1_reg_val |= *tx_ptr & 0xFF;
            tx_ptr++;
        }
        
        /* Write to SPIDAT1 */
        if((i == (nbytes -1)) && (terminate)) 
        {
            /* Release the CS at the end of the transfer when terminate flag is TRUE */
            SPI_SPIDAT1 = data1_reg_val & ~(CSL_SPI_SPIDAT1_CSHOLD_ENABLE << CSL_SPI_SPIDAT1_CSHOLD_SHIFT);
        } else 
        {
            SPI_SPIDAT1 = data1_reg_val;
        }
        
        
        /* Read SPIBUF, wait untill the RX buffer is not empty */
        while ( SPI_SPIBUF & ( CSL_SPI_SPIBUF_RXEMPTY_MASK ) );
        
        /* Read one byte data */
        buf_reg = SPI_SPIBUF;
        if(rx_ptr) 
        {
            *rx_ptr = buf_reg & 0xFF;
            rx_ptr++;
        }
    }
    
    return SPI_EOK;
    
}


/******************************************************************************
 * 
 * Function:    spi_cmd  
 *
 * Description: This function sends a single byte command and receives response data
 *
 * Parameters:  uint8_t  cmd      - Command sent to the NOR flash
 *              uint8_t* response - Pointer to the RX response data
 *              uint32_t len      - Lenght of the response in bytes
 *
 * Return Value: error status
 * 
 ******************************************************************************/
SPI_STATUS 
spi_cmd
(
    uint8_t               cmd,
    uint8_t*              response,
    uint32_t              len
)
{
    Bool        flags = FALSE;
    uint32_t      ret;
    
    if (len == 0)
    {
        flags = TRUE;
    }
    
    /* Send the command byte */
    ret = spi_xfer(1, &cmd, NULL, flags);
    if (ret) 
    {
    	IFPRINT (platform_write("SF: Failed to send command %02x: %d\n", cmd, ret));
        return ret;
    }
    
    /* Receive the response */
    if (len) 
    {
        ret = spi_xfer(len, NULL, response, TRUE);
        if (ret)
        {
        	IFPRINT (platform_write("SF: Failed to read response (%zu bytes): %d\n",  len, ret));
        }
    }
    
    return ret;
}

/******************************************************************************
 * 
 * Function:    spi_cmd_read  
 *
 * Description: This function sends a read command and reads data from the flash
 *
 * Parameters:  uint8_t  cmd      - Command sent to the NOR flash
 *              uint32_t cmd_len  - Length of the command in bytes
 *              uint8_t* dat      - Pointer to the data read
 *              uint32_t data_len - Lenght of the data read in bytes
 *
 * Return Value: error status
 * 
 ******************************************************************************/
SPI_STATUS 
spi_cmd_read
(
    uint8_t*              cmd,
    uint32_t              cmd_len,
    uint8_t*              data,
    uint32_t              data_len
)
{
    Bool        flags = FALSE;
    uint32_t      ret;
    
    if (data_len == 0)
    {
        flags = TRUE;
    }

    /* Send read command */
    ret = spi_xfer(cmd_len, cmd, NULL, flags);
    if (ret) 
    {
    	IFPRINT (platform_write("SF: Failed to send read command (%zu bytes): %d\n",
               cmd_len, ret));
    } 
    else if (data_len != 0) 
    {
        /* Read data */
        ret = spi_xfer(data_len, NULL, data, TRUE);
        if (ret)
        {
        	IFPRINT (platform_write("SF: Failed to read %zu bytes of data: %d\n",
                   data_len, ret));
        }
    }
    
    return ret;
}

/******************************************************************************
 * 
 * Function:    spi_cmd_write  
 *
 * Description: This function sends a write command and writes data to the flash
 *
 * Parameters:  uint8_t  cmd      - Command sent to the NOR flash
 *              uint32_t cmd_len  - Length of the command in bytes
 *              uint8_t* dat      - Pointer to the data to be written
 *              uint32_t data_len - Lenght of the data in bytes
 *
 * Return Value: error status
 * 
 ******************************************************************************/
SPI_STATUS 
spi_cmd_write
(
    uint8_t*        cmd,
    uint32_t        cmd_len,
    uint8_t*        data,
    uint32_t        data_len
)
{
    Bool           flags = FALSE;
    uint32_t         ret;
    
    if (data_len == 0)
    {
        flags = TRUE;
    }
    
    /* Send write command */
    ret = spi_xfer(cmd_len, cmd, NULL, flags);
    if (ret) 
    {
    	IFPRINT (platform_write("SF: Failed to send write command (%zu bytes): %d\n",
            cmd_len, ret));
    } 
    else if (data_len != 0) 
    {
        /* Write data */
        ret = spi_xfer(data_len, data, NULL, TRUE);
        if (ret)
        {
        	IFPRINT (platform_write("SF: Failed to write %zu bytes of data: %d\n",
            data_len, ret));
        }
    }
    
    return ret;
}


/******************************************************************************
 * 
 * Function:    spi_read_word  
 *
 * Description: This function sends a read command and reads data in 16-bit data format  
 *
 * Parameters:  uint16_t* cmd_buf  - Pointer to the command sent
 *              uint32_t cmd_len   - Length of the command in words
 *              uint16_t* data_buf - Pointer to the data read
 *              uint32_t data_len  - Lenght of the data read in words
 *
 * Return Value: error status
 * 
 ******************************************************************************/
SPI_STATUS 
spi_read_word
(
    uint16_t*             cmd_buf,
    uint32_t              cmd_len,
    uint16_t*             data_buf,
    uint32_t              data_len
)
{
    uint32_t          data1_reg;
    uint16_t*         tx_ptr = cmd_buf;
    uint16_t*         rx_ptr = data_buf;
    
	/* disable the SPI communication by setting 
	 * the SPIGCR1.ENABLE to 0 
	 * 
	 * 
	 * SPIGCR1
	 * ============================================
	 * Bit 	Field 	Value 		Description
	 * 24 	ENABLE 	0			SPI disable
	 * ============================================
	 */
	data1_reg = 0x1 << 24;
	data1_reg = ~data1_reg;
    SPI_SPIGCR1 &= data1_reg;

	/*
	 * clean TX data into SPIDAT0
	 * 
	 * SPIDAT0
	 * ============================================
	 * Bit 	Field 	Value 		Description
	 * 15-0 TXDATA 	0-FFFFh 	SPI transmit data
	 * ============================================
	 * 
	 */

    SPI_SPIDAT0 = 0;

	/* 8.
	 * Enable the SPI communication by setting 
	 * the SPIGCR1.ENABLE to 1 
	 * 
	 * 
	 * SPIGCR1
	 * ============================================
	 * Bit 	Field 	Value 		Description
	 * 24 	ENABLE 	1			SPI enable
	 * ============================================
	 */

	data1_reg = 0x1 << 24;
    SPI_SPIGCR1 = (SPI_SPIGCR1 | data1_reg);    
    
    {
        {
            SPI_SPIDAT0 = *tx_ptr;
            spi_delay(10000);
        }

        /* Read SPIFLG, wait untill the RX full interrupt */
        if ( (SPI_SPIFLG & (CSL_SPI_SPIFLG_RXINTFLG_FULL<<CSL_SPI_SPIFLG_RXINTFLG_SHIFT)) ) {                
            /* Read one byte data */
            *rx_ptr = SPI_SPIBUF & 0xFF;
            SPI_SPIBUF = 0;
        }
        else {
            return SPI_EFAIL;
        }
        
    }
    
    return SPI_EOK;

}

/******************************************************************************
 * 
 * Function:    spi_write_word  
 *
 * Description: This function sends a write command and writes data in 16-bit data format 
 *
 * Parameters:  uint16_t* cmd_buf  - Pointer to the command sent
 *              uint32_t cmd_len   - Length of the command in bytes
 *              uint16_t* data_buf - Pointer to the data read
 *              uint32_t data_len  - Lenght of the data read in bytes
 *
 * Return Value: error status
 * 
 ******************************************************************************/
SPI_STATUS 
spi_write_word
(
    uint16_t*             cmd_buf,
    uint32_t              cmd_len,
    uint16_t*             data_buf,
    uint32_t              data_len
)
{
    uint32_t          data1_reg;
    uint16_t*         tx_ptr = cmd_buf;

	/* disable the SPI communication by setting 
	 * the SPIGCR1.ENABLE to 0 
	 * 
	 * 
	 * SPIGCR1
	 * ============================================
	 * Bit 	Field 	Value 		Description
	 * 24 	ENABLE 	0			SPI disable
	 * ============================================
	 */
	data1_reg = 0x1 << 24;
	data1_reg = ~data1_reg;
    SPI_SPIGCR1 &= data1_reg;

	/*
	 * clean TX data into SPIDAT0
	 * 
	 * SPIDAT0
	 * ============================================
	 * Bit 	Field 	Value 		Description
	 * 15-0 TXDATA 	0-FFFFh 	SPI transmit data
	 * ============================================
	 * 
	 */

    SPI_SPIDAT0 = 0;

	/* 8.
	 * Enable the SPI communication by setting 
	 * the SPIGCR1.ENABLE to 1 
	 * 
	 * 
	 * SPIGCR1
	 * ============================================
	 * Bit 	Field 	Value 		Description
	 * 24 	ENABLE 	1			SPI enable
	 * ============================================
	 */

	data1_reg = 0x1 << 24;
    SPI_SPIGCR1 = (SPI_SPIGCR1 | data1_reg);    
    
    {
        {
            SPI_SPIDAT0 = *tx_ptr;
            spi_delay(10000);
        }

        /* Read SPIFLG, wait untill the RX full interrupt */
        if ( (SPI_SPIFLG & (CSL_SPI_SPIFLG_TXINTFLG_EMPTY<<CSL_SPI_SPIFLG_TXINTFLG_SHIFT)) ) {                
            /* Clear the SPIBUF */
            SPI_SPIBUF = 0;
            return SPI_EOK;
        }
        else {
            return SPI_EFAIL;
        }
        
    }
}


/**
 *  \file   main_spi_flash_read_example.c
 *
 *  \brief  Example application main file. This application will read
 *          the data from flash through spi interface.
 *
 */

/*
 * Copyright (C) 2015 - 2018 Texas Instruments Incorporated - http://www.ti.com/
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * Redistributions of source code must retain the above copyright
 * notice, this list of conditions and the following disclaimer.
 *
 * Redistributions in binary form must reproduce the above copyright
 * notice, this list of conditions and the following disclaimer in the
 * documentation and/or other materials provided with the
 * distribution.
 *
 * Neither the name of Texas Instruments Incorporated nor the names of
 * its contributors may be used to endorse or promote products derived
 * from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
 * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
 * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
 * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
 * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
 * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
 * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
 * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
 * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
 * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
 * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 *
 */

#ifndef BARE_METAL
/* XDCtools Header files */
#include <xdc/std.h>
#include <xdc/cfg/global.h>
#include <xdc/runtime/System.h>
#include <stdio.h>

/* BIOS Header files */
#include <ti/sysbios/BIOS.h>
#endif

/* SPI Header files */
#include <ti/drv/spi/SPI.h>
#if defined(SOC_K2H) || defined(SOC_K2K) || defined(SOC_K2E) || defined(SOC_K2L) || defined(SOC_K2G) || defined(SOC_C6678) || defined(SOC_C6657) || defined(SOC_OMAPL137) || defined(SOC_OMAPL138)
#include <ti/drv/spi/src/v0/SPI_v0.h>
#endif
#include <ti/drv/spi/soc/SPI_soc.h>
#include <ti/drv/spi/test/src/SPI_log.h>
#include <ti/drv/spi/test/src/SPI_test.h>

/* Board Header files */
#include <ti/board/board.h>
#include <ti/board/src/flash/include/board_flash.h>

/**********************************************************************
 ************************** Macros ************************************
 **********************************************************************/

/**********************************************************************
 ************************** Internal functions ************************
 **********************************************************************/

/**********************************************************************
 ************************** Global Variables **************************
 **********************************************************************/

/* Buffer containing the received data */
uint8_t rxBuf[TEST_TX_LENGTH];

/* transfer length */
uint32_t transferLength;

/*
 *  ======== Board_initSPI ========
 */
void Board_initSPI(void)
{
    Board_initCfg boardCfg;
#if defined(SOC_K2H) || defined(SOC_K2K) || defined(SOC_K2E) || defined(SOC_K2L) || defined(SOC_K2G) || defined(SOC_C6678) || defined(SOC_C6657) || defined(SOC_OMAPL137) || defined(SOC_OMAPL138)
    SPI_v0_HWAttrs spi_cfg;
    Board_SoCInfo socInfo;

    /* Get the default SPI init configurations */
    SPI_socGetInitCfg(TEST_SPI_PORT, &spi_cfg);

    /* Update the SPI functional clock based on CPU clock*/
    Board_getSoCInfo(&socInfo);
    if(socInfo.sysClock != BOARD_SYS_CLK_DEFAULT)
    {
        spi_cfg.inputClkFreq = socInfo.sysClock/SPI_MODULE_CLOCK_DIVIDER;
    }

    /* Set the default SPI init configurations */
    SPI_socSetInitCfg(TEST_SPI_PORT, &spi_cfg);
#endif

#if defined(evmK2E) || defined(evmC6678)
    boardCfg = BOARD_INIT_MODULE_CLOCK |
        BOARD_INIT_UART_STDIO;
#else
    boardCfg = BOARD_INIT_PINMUX_CONFIG |
        BOARD_INIT_MODULE_CLOCK |
        BOARD_INIT_UART_STDIO;
#endif
    Board_init(boardCfg);
}


/*
 *  ======== test function ========
 */
#ifdef BARE_METAL
void main()
#else
void spi_test(UArg arg0, UArg arg1)
#endif
{
    Board_flashHandle  boardHandle;
    Board_FlashInfo   *flashInfo;
    uint32_t           blockNum, pageNum;
    SPI_Params       spiParams;                        /* SPI params structure */
    bool               testPassed = true;

#ifdef BARE_METAL
    /* Call board init functions */
    Board_initSPI();
#endif

    /* Open the Board flash NOR device with the test SPI port
       and use the default SPI configurations */
    SPI_Params_init(&spiParams);
    spiParams.frameFormat  = SPI_POL0_PHA1;
    boardHandle = Board_flashOpen(TEST_NOR_DEV_ID,
                                  TEST_SPI_PORT,
                                  (void *)(&spiParams));
    if (!boardHandle)
    {
        SPI_log("\n Board_flashOpen failed. \n");
        goto err;
    }
    else
    {
        flashInfo = (Board_FlashInfo *)boardHandle;
        SPI_log("\n SPI NOR device ID: 0x%x, manufacturer ID: 0x%x \n",
                flashInfo->device_id, flashInfo->manufacturer_id);
    }

    if (Board_flashOffsetToBlkPage(boardHandle, TEST_NOR_ADDR,
                                   &blockNum, &pageNum))
    {
        SPI_log("\n Board_flashOffsetToBlkPage failed. \n");
        testPassed = false;
        goto err;
    }

    /* Set the transfer length in number of 32 bit words */
    transferLength = TEST_TX_LENGTH;

    /* Read data from flash */
    if (Board_flashRead(boardHandle, TEST_NOR_ADDR, (uint8_t *)&rxBuf[0],
                        TEST_TX_LENGTH, NULL))
    {
        SPI_log("\n Board_flashRead failed. \n");
        testPassed = false;
        goto err;
    }

    Board_flashClose(boardHandle);

err:
    if(true == testPassed)
    {
        SPI_log("\n All tests have passed. \n");
    }
    else
    {
        SPI_log("\n Some tests have failed. \n");
    }

    while(1);
}

/*
 *  ======== main ========
 */
#ifndef BARE_METAL
int main(void)
{
    /* Call board init functions */
    Board_initSPI();

    /* Start BIOS */
    BIOS_start();
    return (0);
}
#endif

I am using Processor SDK 5.2 for this purpose. I went to some of the e2e posts but didnt find anything for my reference.  If anybody can refer to me in the right direction that would be really helpful.

Thanks

Harshul